<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using machine learning with a simple yocto project image in eIQ Machine Learning Software</title>
    <link>https://community.nxp.com/t5/eIQ-Machine-Learning-Software/Using-machine-learning-with-a-simple-yocto-project-image/m-p/1343401#M478</link>
    <description>&lt;P&gt;I would like to know if it is possible to use machine learning software (my device is the&amp;nbsp;i.MX 8 M mini). I want to know if i can do that building only the&amp;nbsp;core-image-base Yocto Project image or an image more simple than the full one (the one recommended for ML). We have a console based device.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Tue, 21 Sep 2021 16:37:39 GMT</pubDate>
    <dc:creator>Olatz</dc:creator>
    <dc:date>2021-09-21T16:37:39Z</dc:date>
    <item>
      <title>Using machine learning with a simple yocto project image</title>
      <link>https://community.nxp.com/t5/eIQ-Machine-Learning-Software/Using-machine-learning-with-a-simple-yocto-project-image/m-p/1343401#M478</link>
      <description>&lt;P&gt;I would like to know if it is possible to use machine learning software (my device is the&amp;nbsp;i.MX 8 M mini). I want to know if i can do that building only the&amp;nbsp;core-image-base Yocto Project image or an image more simple than the full one (the one recommended for ML). We have a console based device.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Tue, 21 Sep 2021 16:37:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/eIQ-Machine-Learning-Software/Using-machine-learning-with-a-simple-yocto-project-image/m-p/1343401#M478</guid>
      <dc:creator>Olatz</dc:creator>
      <dc:date>2021-09-21T16:37:39Z</dc:date>
    </item>
  </channel>
</rss>