<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic how to change input size of the base model on eIQ software in eIQ Machine Learning Software</title>
    <link>https://community.nxp.com/t5/eIQ-Machine-Learning-Software/how-to-change-input-size-of-the-base-model-on-eIQ-software/m-p/1337059#M454</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I was planning on training a model that requires 640x640 of input image size, but the base models eIQ software only supports 320x320 input size. So I decided to modify the input layer of the base model to 640x640 such that I can avoid training it with 320x320(the base model is "C:\nxp\eIQ_Toolkit_v1.0.5\plugins\detection\boxes\fpn\VOC-fpn_ssd_mobilenet_v2-320.h5"). Is this a recommended approach in general and also how can I achieve this goal? Thanks very much!&lt;/P&gt;</description>
    <pubDate>Wed, 08 Sep 2021 18:16:53 GMT</pubDate>
    <dc:creator>jasonliu1</dc:creator>
    <dc:date>2021-09-08T18:16:53Z</dc:date>
    <item>
      <title>how to change input size of the base model on eIQ software</title>
      <link>https://community.nxp.com/t5/eIQ-Machine-Learning-Software/how-to-change-input-size-of-the-base-model-on-eIQ-software/m-p/1337059#M454</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I was planning on training a model that requires 640x640 of input image size, but the base models eIQ software only supports 320x320 input size. So I decided to modify the input layer of the base model to 640x640 such that I can avoid training it with 320x320(the base model is "C:\nxp\eIQ_Toolkit_v1.0.5\plugins\detection\boxes\fpn\VOC-fpn_ssd_mobilenet_v2-320.h5"). Is this a recommended approach in general and also how can I achieve this goal? Thanks very much!&lt;/P&gt;</description>
      <pubDate>Wed, 08 Sep 2021 18:16:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/eIQ-Machine-Learning-Software/how-to-change-input-size-of-the-base-model-on-eIQ-software/m-p/1337059#M454</guid>
      <dc:creator>jasonliu1</dc:creator>
      <dc:date>2021-09-08T18:16:53Z</dc:date>
    </item>
  </channel>
</rss>