<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>eIQ Machine Learning Software中的主题 OpenCV cuda imgproc library</title>
    <link>https://community.nxp.com/t5/eIQ-Machine-Learning-Software/OpenCV-cuda-imgproc-library/m-p/1315376#M388</link>
    <description>&lt;P&gt;I am using OpenCV (4.5.2) on an i.MX8MQ. I am having slow performance using the matchTemplate function. I see there is a GPU hardware accelerated TemplateMatching version in the cv::cuda namespace. I am building w/YOCTO linux L5.10.35_2.2.0 using the imx-image-full which pretty much builds in everything including OpenCV 4.5.2. I can see a few cuda headers in the /usr/include/opencv4/opencv2/core/cuda but not the cuda based imageproc ones.&lt;/P&gt;&lt;P&gt;Is this incomplete? Is it possible to build in the additional cuda libraries? will they be GPU accelerated?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 29 Jul 2021 15:23:10 GMT</pubDate>
    <dc:creator>davidvescovi</dc:creator>
    <dc:date>2021-07-29T15:23:10Z</dc:date>
    <item>
      <title>OpenCV cuda imgproc library</title>
      <link>https://community.nxp.com/t5/eIQ-Machine-Learning-Software/OpenCV-cuda-imgproc-library/m-p/1315376#M388</link>
      <description>&lt;P&gt;I am using OpenCV (4.5.2) on an i.MX8MQ. I am having slow performance using the matchTemplate function. I see there is a GPU hardware accelerated TemplateMatching version in the cv::cuda namespace. I am building w/YOCTO linux L5.10.35_2.2.0 using the imx-image-full which pretty much builds in everything including OpenCV 4.5.2. I can see a few cuda headers in the /usr/include/opencv4/opencv2/core/cuda but not the cuda based imageproc ones.&lt;/P&gt;&lt;P&gt;Is this incomplete? Is it possible to build in the additional cuda libraries? will they be GPU accelerated?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jul 2021 15:23:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/eIQ-Machine-Learning-Software/OpenCV-cuda-imgproc-library/m-p/1315376#M388</guid>
      <dc:creator>davidvescovi</dc:creator>
      <dc:date>2021-07-29T15:23:10Z</dc:date>
    </item>
  </channel>
</rss>