<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic pyeiq for 5.4.70_2.3.0 BSP in eIQ Machine Learning Software</title>
    <link>https://community.nxp.com/t5/eIQ-Machine-Learning-Software/pyeiq-for-5-4-70-2-3-0-BSP/m-p/1209811#M338</link>
    <description>&lt;P&gt;Dear Mr. Dorta,&lt;/P&gt;&lt;P&gt;When will the newest pyeiq be available for the latest NXP imx BSP ? (5.4.70_2.3.0) It was published last year, long ago. As you know the current pyeiq does not work with the new BSP. For example the executables were linked against libopencv4.2 libraries.&lt;/P&gt;&lt;P&gt;Will it be opensource framework at last ? Or you want to keep it partially closed source ? As you know it downloades executables and models from the net. If the execurable won't find libopencv4.2, it can't run. If there is no source it can't be rebuilt. And the user gets stuck. This is maybe not the most efficient way to install and run a demo, at least this is not an opensource linux style framework&lt;/P&gt;&lt;P&gt;We can see demos on the home page:&amp;nbsp;&lt;A href="https://pyeiq.dev/" target="_blank"&gt;https://pyeiq.dev/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Some gif pictures show us object detections, object classifications. Are those video files available ? (room.mp4, street.mp4) and the models for them and maybe the command line you executed to create those ml demos ?&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Laci&lt;/P&gt;</description>
    <pubDate>Mon, 11 Jan 2021 17:37:22 GMT</pubDate>
    <dc:creator>lacitele</dc:creator>
    <dc:date>2021-01-11T17:37:22Z</dc:date>
    <item>
      <title>pyeiq for 5.4.70_2.3.0 BSP</title>
      <link>https://community.nxp.com/t5/eIQ-Machine-Learning-Software/pyeiq-for-5-4-70-2-3-0-BSP/m-p/1209811#M338</link>
      <description>&lt;P&gt;Dear Mr. Dorta,&lt;/P&gt;&lt;P&gt;When will the newest pyeiq be available for the latest NXP imx BSP ? (5.4.70_2.3.0) It was published last year, long ago. As you know the current pyeiq does not work with the new BSP. For example the executables were linked against libopencv4.2 libraries.&lt;/P&gt;&lt;P&gt;Will it be opensource framework at last ? Or you want to keep it partially closed source ? As you know it downloades executables and models from the net. If the execurable won't find libopencv4.2, it can't run. If there is no source it can't be rebuilt. And the user gets stuck. This is maybe not the most efficient way to install and run a demo, at least this is not an opensource linux style framework&lt;/P&gt;&lt;P&gt;We can see demos on the home page:&amp;nbsp;&lt;A href="https://pyeiq.dev/" target="_blank"&gt;https://pyeiq.dev/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Some gif pictures show us object detections, object classifications. Are those video files available ? (room.mp4, street.mp4) and the models for them and maybe the command line you executed to create those ml demos ?&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Laci&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jan 2021 17:37:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/eIQ-Machine-Learning-Software/pyeiq-for-5-4-70-2-3-0-BSP/m-p/1209811#M338</guid>
      <dc:creator>lacitele</dc:creator>
      <dc:date>2021-01-11T17:37:22Z</dc:date>
    </item>
  </channel>
</rss>