<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>eIQ Machine Learning Softwareのトピックbuild eIQ image failed</title>
    <link>https://community.nxp.com/t5/eIQ-Machine-Learning-Software/build-eIQ-image-failed/m-p/1150801#M294</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I'm building an eIQ image for my imx8mqevk and encountered an issue as following....&lt;BR /&gt;what should i do?&lt;/P&gt;&lt;P&gt;OS : Ubuntu16.04 in VMware&amp;nbsp;&lt;/P&gt;&lt;P&gt;ERROR: tensorflow-1.12.0-r0 do_configure: Function failed: do_configure (log file is located at /home/stu/fsl-arm-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/tensorflow/1.12.0-r0/temp/log.do_configure.84900)&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/stu/fsl-arm-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/tensorflow/1.12.0-r0/temp/log.do_configure.84900&lt;BR /&gt;Log data follows:&lt;BR /&gt;| DEBUG: Executing shell function do_configure&lt;BR /&gt;| downloading &lt;A href="https://bitbucket.org/eigen/eigen/get/fd6845384b86.tar.gz" target="_blank"&gt;https://bitbucket.org/eigen/eigen/get/fd6845384b86.tar.gz&lt;/A&gt;&lt;BR /&gt;|&lt;BR /&gt;| gzip: stdin: unexpected end of file&lt;BR /&gt;| tar: Child returned status 1&lt;BR /&gt;| tar: Error is not recoverable: exiting now&lt;BR /&gt;| WARNING: exit code 2 from a shell command.&lt;BR /&gt;| &lt;FONT color="#FF0000"&gt;ERROR: Function failed: do_configure (log file is located at /home/stu/fsl-arm-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/tensorflow/1.12.0-r0/temp/log.do_configure.84900)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;ERROR: Task (/home/stu/fsl-arm-yocto-bsp/sources/meta-imx-machinelearning/recipes-libraries/tensorflow/tensorflow_1.12.0.bb:do_configure) failed with exit code '1'&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;NOTE: Tasks Summary: Attempted 6041 tasks of which 0 didn't need to be rerun and 1 failed.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;Summary: 1 task failed:&lt;BR /&gt;/home/stu/fsl-arm-yocto-bsp/sources/meta-imx-machinelearning/recipes-libraries/tensorflow/tensorflow_1.12.0.bb:do_configure&lt;BR /&gt;Summary: There were 14 WARNING messages shown.&lt;BR /&gt;Summary: There was 1 ERROR message shown, returning a non-zero exit code.&lt;/P&gt;</description>
    <pubDate>Wed, 09 Sep 2020 05:27:34 GMT</pubDate>
    <dc:creator>g0930421313</dc:creator>
    <dc:date>2020-09-09T05:27:34Z</dc:date>
    <item>
      <title>build eIQ image failed</title>
      <link>https://community.nxp.com/t5/eIQ-Machine-Learning-Software/build-eIQ-image-failed/m-p/1150801#M294</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I'm building an eIQ image for my imx8mqevk and encountered an issue as following....&lt;BR /&gt;what should i do?&lt;/P&gt;&lt;P&gt;OS : Ubuntu16.04 in VMware&amp;nbsp;&lt;/P&gt;&lt;P&gt;ERROR: tensorflow-1.12.0-r0 do_configure: Function failed: do_configure (log file is located at /home/stu/fsl-arm-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/tensorflow/1.12.0-r0/temp/log.do_configure.84900)&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/stu/fsl-arm-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/tensorflow/1.12.0-r0/temp/log.do_configure.84900&lt;BR /&gt;Log data follows:&lt;BR /&gt;| DEBUG: Executing shell function do_configure&lt;BR /&gt;| downloading &lt;A href="https://bitbucket.org/eigen/eigen/get/fd6845384b86.tar.gz" target="_blank"&gt;https://bitbucket.org/eigen/eigen/get/fd6845384b86.tar.gz&lt;/A&gt;&lt;BR /&gt;|&lt;BR /&gt;| gzip: stdin: unexpected end of file&lt;BR /&gt;| tar: Child returned status 1&lt;BR /&gt;| tar: Error is not recoverable: exiting now&lt;BR /&gt;| WARNING: exit code 2 from a shell command.&lt;BR /&gt;| &lt;FONT color="#FF0000"&gt;ERROR: Function failed: do_configure (log file is located at /home/stu/fsl-arm-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/tensorflow/1.12.0-r0/temp/log.do_configure.84900)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;ERROR: Task (/home/stu/fsl-arm-yocto-bsp/sources/meta-imx-machinelearning/recipes-libraries/tensorflow/tensorflow_1.12.0.bb:do_configure) failed with exit code '1'&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;NOTE: Tasks Summary: Attempted 6041 tasks of which 0 didn't need to be rerun and 1 failed.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;Summary: 1 task failed:&lt;BR /&gt;/home/stu/fsl-arm-yocto-bsp/sources/meta-imx-machinelearning/recipes-libraries/tensorflow/tensorflow_1.12.0.bb:do_configure&lt;BR /&gt;Summary: There were 14 WARNING messages shown.&lt;BR /&gt;Summary: There was 1 ERROR message shown, returning a non-zero exit code.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Sep 2020 05:27:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/eIQ-Machine-Learning-Software/build-eIQ-image-failed/m-p/1150801#M294</guid>
      <dc:creator>g0930421313</dc:creator>
      <dc:date>2020-09-09T05:27:34Z</dc:date>
    </item>
  </channel>
</rss>