<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PCA85133 in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA85133/m-p/661411#M999</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No, there are no effects if different voltages are used to supply VDD and VLCD since they are not internally connected, VDD is used as the supply for the internal device functionality, while VLCD is the supply dedicated for pins which interface with the LCD.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Just take in mind that static voltages across the liquid crystal display can build up when the LCD supply voltage (VLCD) is on while the IC supply voltage (VDD) is off, or vice versa. This may cause unwanted display artifacts. To avoid such artifacts, VLCD and VDD must be applied or removed together&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Mar 2017 21:18:13 GMT</pubDate>
    <dc:creator>reyes</dc:creator>
    <dc:date>2017-03-22T21:18:13Z</dc:date>
    <item>
      <title>PCA85133</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA85133/m-p/661410#M998</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;PCA85133的VDD的输入范围为1.8-5.5V,VLCD的输入范围：2.5V-8V;请问不同的电压输入对芯片有什么影响？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Mar 2017 08:32:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA85133/m-p/661410#M998</guid>
      <dc:creator>feiwen</dc:creator>
      <dc:date>2017-03-17T08:32:58Z</dc:date>
    </item>
    <item>
      <title>Re: PCA85133</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA85133/m-p/661411#M999</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No, there are no effects if different voltages are used to supply VDD and VLCD since they are not internally connected, VDD is used as the supply for the internal device functionality, while VLCD is the supply dedicated for pins which interface with the LCD.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Just take in mind that static voltages across the liquid crystal display can build up when the LCD supply voltage (VLCD) is on while the IC supply voltage (VDD) is off, or vice versa. This may cause unwanted display artifacts. To avoid such artifacts, VLCD and VDD must be applied or removed together&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Mar 2017 21:18:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA85133/m-p/661411#M999</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2017-03-22T21:18:13Z</dc:date>
    </item>
  </channel>
</rss>