<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: start up with external oscillator in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/start-up-with-external-oscillator/m-p/642635#M964</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;can you tell me the part number of DSC you are using? anyway, I suggest you use PE to generate the code to use external crystal or clock source, you can select the external crystal in cpu beans.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Oct 2016 07:50:38 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2016-10-26T07:50:38Z</dc:date>
    <item>
      <title>start up with external oscillator</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/start-up-with-external-oscillator/m-p/642634#M963</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi all,&lt;/P&gt;&lt;P&gt;is there a code example how to configure occs if external Crystal oscillator is used?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Oct 2016 16:52:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/start-up-with-external-oscillator/m-p/642634#M963</guid>
      <dc:creator>matthiasuhlmann</dc:creator>
      <dc:date>2016-10-17T16:52:51Z</dc:date>
    </item>
    <item>
      <title>Re: start up with external oscillator</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/start-up-with-external-oscillator/m-p/642635#M964</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;can you tell me the part number of DSC you are using? anyway, I suggest you use PE to generate the code to use external crystal or clock source, you can select the external crystal in cpu beans.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Oct 2016 07:50:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/start-up-with-external-oscillator/m-p/642635#M964</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-10-26T07:50:38Z</dc:date>
    </item>
    <item>
      <title>Re: start up with external oscillator</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/start-up-with-external-oscillator/m-p/642636#M965</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi XiangJun rong,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do not use Processor Expert. Would this generate a useful example?&lt;/P&gt;&lt;P&gt;I will try to generate example....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Matthias&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Oct 2016 10:00:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/start-up-with-external-oscillator/m-p/642636#M965</guid>
      <dc:creator>matthiasuhlmann</dc:creator>
      <dc:date>2016-10-27T10:00:00Z</dc:date>
    </item>
  </channel>
</rss>