<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 56F84789 PWMB  in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/56F84789-PWMB/m-p/631428#M945</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have checked the PE configuration, a lof items are not set. I help you set all the PE configuration, now it is okay.&lt;/P&gt;&lt;P&gt;You can check the PWMB signals from GPIOG0,GPIOG1,GPIOG2,&lt;STRONG&gt;GPIOG3 and GPIOE8 and GPIOE9 pins, if you have TWR-8400 board, you can test the pin4,6,21,22,23,24 of J503 connector.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I attach the project which is based on your project.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;BR&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Xiangjun Rong&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Apr 2017 07:17:47 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2017-04-26T07:17:47Z</dc:date>
    <item>
      <title>56F84789 PWMB</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/56F84789-PWMB/m-p/631425#M942</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello. I have a question about 56F84789. When I use 56F84789,&amp;nbsp;&lt;SPAN style="color: #333333; background-color: #ffffff; font-size: 13px;"&gt;&amp;nbsp;I&amp;nbsp;&lt;/SPAN&gt;&lt;A href="http://www.baidu.com/link?url=kLLwSTek1oAtaj8EqxEsBf5p7QWhxmDc_emDY_VeIpNZBkwejgjgGDcWDpI2SRXnGM-8JErqRh0Yrt1kFpkfy8F3KQo_dzro-9iA7fl9EEe" style="color: #333333; background-color: #ffffff; font-size: 13px;" target="_blank"&gt;configure&lt;/A&gt;&amp;nbsp;the bean PWMMC to generator PWMA and PWMB in Codewarrior. However, I can observe PWMA signal ,but I cannot find PWMB signal. If there are some differences between PWMA and PWMB.Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Apr 2017 03:30:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/56F84789-PWMB/m-p/631425#M942</guid>
      <dc:creator>saideliu</dc:creator>
      <dc:date>2017-04-21T03:30:55Z</dc:date>
    </item>
    <item>
      <title>Re: 56F84789 PWMB</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/56F84789-PWMB/m-p/631426#M943</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Liu,&lt;/P&gt;&lt;P&gt;The main difference of PWMA and PWMB is that the PWMB does not support nano-edge placement feature, the PWMA module supports the nano-edge placement feature. For the other feature, they are the same.&lt;/P&gt;&lt;P&gt;If you still have issue, pls post your project so that we can have a review.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Apr 2017 06:14:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/56F84789-PWMB/m-p/631426#M943</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2017-04-25T06:14:25Z</dc:date>
    </item>
    <item>
      <title>Re: 56F84789 PWMB</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/56F84789-PWMB/m-p/631427#M944</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi！Rong.&lt;/P&gt;&lt;P&gt;I add the project in the attachment. And I found that the register PWMB_FSTS0 =0x0800.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think the bean that configures PWMB may have some mistakes, pls look at the project and find the cause or give a project that uses bean configures PWMB.&lt;/P&gt;&lt;P&gt;Hoping for your reply.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Apr 2017 11:42:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/56F84789-PWMB/m-p/631427#M944</guid>
      <dc:creator>saideliu</dc:creator>
      <dc:date>2017-04-25T11:42:24Z</dc:date>
    </item>
    <item>
      <title>Re: 56F84789 PWMB</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/56F84789-PWMB/m-p/631428#M945</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have checked the PE configuration, a lof items are not set. I help you set all the PE configuration, now it is okay.&lt;/P&gt;&lt;P&gt;You can check the PWMB signals from GPIOG0,GPIOG1,GPIOG2,&lt;STRONG&gt;GPIOG3 and GPIOE8 and GPIOE9 pins, if you have TWR-8400 board, you can test the pin4,6,21,22,23,24 of J503 connector.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I attach the project which is based on your project.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;BR&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Xiangjun Rong&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Apr 2017 07:17:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/56F84789-PWMB/m-p/631428#M945</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2017-04-26T07:17:47Z</dc:date>
    </item>
    <item>
      <title>Re: 56F84789 PWMB</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/56F84789-PWMB/m-p/631429#M946</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your help. According to the project you attached, I found that  Fault channel is configured by no instead of yes. Then I changed the configuration, PWMB worked.Thank you again.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Apr 2017 13:41:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/56F84789-PWMB/m-p/631429#M946</guid>
      <dc:creator>saideliu</dc:creator>
      <dc:date>2017-04-26T13:41:51Z</dc:date>
    </item>
  </channel>
</rss>