<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal ControllersのトピックMC56F8335 program flash size</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8335-program-flash-size/m-p/607942#M882</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i have a question about the MC56F8335 program flash size. The technical data sheet:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fassets%2Fdocuments%2Fdata%2Fen%2Fdata-sheets%2FMC56F8335.pdf" rel="nofollow" target="_blank"&gt;http://www.nxp.com/assets/documents/data/en/data-sheets/MC56F8335.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;says:&lt;/P&gt;&lt;P&gt;* Table 4-1: Program Flash 64kB&lt;/P&gt;&lt;P&gt;* Table 4-4: Internal Program Flash 64kB from P:0x00 0000 to P:0x00 7FFF&lt;/P&gt;&lt;P&gt;I think this is wrong! The right program flash size must be 128kB (from P:0x00 0000 to P:0x 00 FFFF)&lt;/P&gt;&lt;P&gt;Only figure 4-1 shows the wright adress-area (P:0x00 0000 to P:0x00 FFFF) with flash configure field at P:0x00 FFF7 to P:0x00 FFFF. The text in figure 4-1 "64kB" is wrong!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I ordered an MC56F8335 and thougt the program flash size is 64kB. Then i erased the program flash and wrote the configure field at P:0x00 7FF7 to P:0x00 7FFF without securing the flash and without setting the protection-bits&amp;nbsp;and i wondered that the DSP-Code itselfe&amp;nbsp;cannot&amp;nbsp;program the data flash. This is because the flash size is 128kB and the Configure field is at P:0x00 FFF7 to P:0x00 FFFF and after erasing the flash the protection-bits in the configure field are all set. So the flash is protected.&lt;/P&gt;&lt;P&gt;Is this correct?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Friendly regards,&lt;/P&gt;&lt;P&gt;Uli&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Feb 2017 13:04:53 GMT</pubDate>
    <dc:creator>ulrichneumayer</dc:creator>
    <dc:date>2017-02-28T13:04:53Z</dc:date>
    <item>
      <title>MC56F8335 program flash size</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8335-program-flash-size/m-p/607942#M882</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i have a question about the MC56F8335 program flash size. The technical data sheet:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fassets%2Fdocuments%2Fdata%2Fen%2Fdata-sheets%2FMC56F8335.pdf" rel="nofollow" target="_blank"&gt;http://www.nxp.com/assets/documents/data/en/data-sheets/MC56F8335.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;says:&lt;/P&gt;&lt;P&gt;* Table 4-1: Program Flash 64kB&lt;/P&gt;&lt;P&gt;* Table 4-4: Internal Program Flash 64kB from P:0x00 0000 to P:0x00 7FFF&lt;/P&gt;&lt;P&gt;I think this is wrong! The right program flash size must be 128kB (from P:0x00 0000 to P:0x 00 FFFF)&lt;/P&gt;&lt;P&gt;Only figure 4-1 shows the wright adress-area (P:0x00 0000 to P:0x00 FFFF) with flash configure field at P:0x00 FFF7 to P:0x00 FFFF. The text in figure 4-1 "64kB" is wrong!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I ordered an MC56F8335 and thougt the program flash size is 64kB. Then i erased the program flash and wrote the configure field at P:0x00 7FF7 to P:0x00 7FFF without securing the flash and without setting the protection-bits&amp;nbsp;and i wondered that the DSP-Code itselfe&amp;nbsp;cannot&amp;nbsp;program the data flash. This is because the flash size is 128kB and the Configure field is at P:0x00 FFF7 to P:0x00 FFFF and after erasing the flash the protection-bits in the configure field are all set. So the flash is protected.&lt;/P&gt;&lt;P&gt;Is this correct?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Friendly regards,&lt;/P&gt;&lt;P&gt;Uli&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Feb 2017 13:04:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8335-program-flash-size/m-p/607942#M882</guid>
      <dc:creator>ulrichneumayer</dc:creator>
      <dc:date>2017-02-28T13:04:53Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F8335 program flash size</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8335-program-flash-size/m-p/607943#M883</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Uli,&lt;/P&gt;&lt;P&gt;You are right, the program flash is 64KW instead of 64KB, the program flash ranges from P:0x00_0000 to P:0x00_0xFFFF, obviously, it is 64KW or 128KB. So the data sheet is wrong, I will notify docmentation team of the issue.&lt;/P&gt;&lt;P&gt;soory for the inconvenience.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Mar 2017 03:27:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8335-program-flash-size/m-p/607943#M883</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2017-03-02T03:27:51Z</dc:date>
    </item>
  </channel>
</rss>