<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RE: TWR-56F8400 module and JTAG debug module CWH-UTP-ONCE  in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/RE-TWR-56F8400-module-and-JTAG-debug-module-CWH-UTP-ONCE/m-p/599887#M852</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The CWH-UTP-ONCE device can be used to debug both MC56F83xx and MC56F84xxx, the blocked pin on the JTAG connector of the CWH-UTP-ONCE device is to avoid that the JTAG connector is inserted reversely. The RED line of the 14 pin cable is the pin1 for the CWH-UTP-ONCE device.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Jan 2017 04:05:38 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2017-01-13T04:05:38Z</dc:date>
    <item>
      <title>RE: TWR-56F8400 module and JTAG debug module CWH-UTP-ONCE</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/RE-TWR-56F8400-module-and-JTAG-debug-module-CWH-UTP-ONCE/m-p/599886#M851</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I believe the JTAG debug module CWH-UTP-ONCE that we use with the 56F8367 should work with the TWR-56F8400 - however, the 14 pin header has all 14 pins present whereas the ONCE connector has one pin blocked. Is the ONCE compatible if we cut the corresponding pin?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jan 2017 22:42:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/RE-TWR-56F8400-module-and-JTAG-debug-module-CWH-UTP-ONCE/m-p/599886#M851</guid>
      <dc:creator>x31</dc:creator>
      <dc:date>2017-01-09T22:42:24Z</dc:date>
    </item>
    <item>
      <title>Re: RE: TWR-56F8400 module and JTAG debug module CWH-UTP-ONCE</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/RE-TWR-56F8400-module-and-JTAG-debug-module-CWH-UTP-ONCE/m-p/599887#M852</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The CWH-UTP-ONCE device can be used to debug both MC56F83xx and MC56F84xxx, the blocked pin on the JTAG connector of the CWH-UTP-ONCE device is to avoid that the JTAG connector is inserted reversely. The RED line of the 14 pin cable is the pin1 for the CWH-UTP-ONCE device.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jan 2017 04:05:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/RE-TWR-56F8400-module-and-JTAG-debug-module-CWH-UTP-ONCE/m-p/599887#M852</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2017-01-13T04:05:38Z</dc:date>
    </item>
    <item>
      <title>Re: RE: TWR-56F8400 module and JTAG debug module CWH-UTP-ONCE</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/RE-TWR-56F8400-module-and-JTAG-debug-module-CWH-UTP-ONCE/m-p/599888#M853</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Xiangjun, Thank You.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I have verified the&amp;nbsp;&lt;SPAN&gt;CWH-UTP-ONCE device does work. We cut pin 8 from the JTAG connector.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;Len&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jan 2017 14:29:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/RE-TWR-56F8400-module-and-JTAG-debug-module-CWH-UTP-ONCE/m-p/599888#M853</guid>
      <dc:creator>x31</dc:creator>
      <dc:date>2017-01-19T14:29:32Z</dc:date>
    </item>
  </channel>
</rss>