<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC56F84452 ADC Accuracy in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F84452-ADC-Accuracy/m-p/491881#M722</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Plinio,&lt;/P&gt;&lt;P&gt;Pls refer to the section 8.5.1 in data sheet of MC56F844xx.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/112790i81EBF5D8527818C5/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Jun 2020 10:20:45 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2020-06-15T10:20:45Z</dc:date>
    <item>
      <title>MC56F84452 ADC Accuracy</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F84452-ADC-Accuracy/m-p/491877#M718</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Last week I observed an interesting behavior in the 12 bit ADC of the MC56F84452.&amp;nbsp; One of the pins that was being measured by the 12 bit ADC was reading a 2.24V signal about 150mV low.&amp;nbsp; My initial thought was that the input was being sampled too fast even though there was very little impedence on the input.&amp;nbsp; So I set the sampling time to the slowest possible time.&amp;nbsp; This did not help.&amp;nbsp; So I made the sample and conversion time faster.&amp;nbsp; This made the sample more accurate.&amp;nbsp; So I made the sample time slower and left the conversion time at the faster level.&amp;nbsp; Accuracy was the same.&amp;nbsp; Slowed the conversion time down and accuracy dropped again.&amp;nbsp; Any ideas on why a faster conversion time would result in a better more accuracy result.&amp;nbsp; The accuracy on the other pins stayed about the same which were good to begin with.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After the sample time, could there be internal leakage on this pin during the conversion time?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is pin 28 (56F84452VLH) which is GPIOB3/ANB3/VREFLB/CMPC_M0.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Apr 2016 12:16:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F84452-ADC-Accuracy/m-p/491877#M718</guid>
      <dc:creator>ee_dugan</dc:creator>
      <dc:date>2016-04-11T12:16:52Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F84452 ADC Accuracy</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F84452-ADC-Accuracy/m-p/491878#M719</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a similar issue with the same part. If I connect the analog input to the VSSA the readings aren't zero but floats around 20 units which translates to (20/4095)*3.3 =&amp;nbsp;16.1172 mV. I also played a little bit with the sampling time and conversion time but it didn't help.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can't think of the cause for this since I'm connected to the reference of the ADC and any noise there should be cancelled when sampling.&lt;/P&gt;&lt;P&gt;Any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jan 2018 04:46:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F84452-ADC-Accuracy/m-p/491878#M719</guid>
      <dc:creator>plinioandrade</dc:creator>
      <dc:date>2018-01-19T04:46:58Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F84452 ADC Accuracy</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F84452-ADC-Accuracy/m-p/491879#M720</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Douglas,&lt;/P&gt;&lt;P&gt;For your issue that only the pin 28 (56F84452VLH) which is GPIOB3/ANB3/VREFLB/CMPC_M0 has issue, because the pin is share with ANB3 and VREFLB function, maybe the VrefLB function has impact on the accuracy. But the errata does not mention the issue.&lt;/P&gt;&lt;P&gt;Hi, Plinio,&lt;/P&gt;&lt;P&gt;It seems that your issue is different with the issue of Douglas, you observe that all channels have the 20 LSB noise issue, for the case, pls check the ADC_RESULT register format:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/35264i1BE89FF5CB004AD1/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;As you can see that the 3 low bit are always 0, if you connect AGND to analog channel, the ADC12_RSLTx is 20 LSB, the actual lsb is about 2~3 bits(20&amp;gt;&amp;gt;3), the noise is about 3mV, i think it is okay. If it is not your case, pls check the ADC driving clock, which must be less than 20MHz.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Feb 2018 09:11:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F84452-ADC-Accuracy/m-p/491879#M720</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2018-02-01T09:11:28Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F84452 ADC Accuracy</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F84452-ADC-Accuracy/m-p/491880#M721</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Xiangjun,&lt;/P&gt;&lt;P&gt;The 20 counts in the ADC was already considering the shift that you talked about above.&lt;/P&gt;&lt;P&gt;Where did you find the information about the ADC driving clock having to be less than 20 MHz?&lt;/P&gt;&lt;P&gt;Sincerely,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jun 2020 05:23:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F84452-ADC-Accuracy/m-p/491880#M721</guid>
      <dc:creator>plinioandrade</dc:creator>
      <dc:date>2020-06-12T05:23:14Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F84452 ADC Accuracy</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F84452-ADC-Accuracy/m-p/491881#M722</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Plinio,&lt;/P&gt;&lt;P&gt;Pls refer to the section 8.5.1 in data sheet of MC56F844xx.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/112790i81EBF5D8527818C5/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jun 2020 10:20:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F84452-ADC-Accuracy/m-p/491881#M722</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-06-15T10:20:45Z</dc:date>
    </item>
  </channel>
</rss>