<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal Controllers中的主题 Re: MWCT1001A for Auto Wireless Charging</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MWCT1001A-for-Auto-Wireless-Charging/m-p/470303#M636</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Kyle,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Of course, the MWCT1001A has internal 8MHz relaxation oscillator, it is the default clock in the source code, after reset, the default 8mhz relaxation oscillator clock is used. If you use internal 8MHz clock, do not use external crystal, you should set CLK_MODE bit as 1(External clock bypass mode) and set the COHL as 1(low power mode to save power) , the two pins GPIOC0/EXTAL, GPIOC1/XTAL can be configured as GPIO pins and external crystal is disabled.&lt;/P&gt;&lt;P&gt;Hope it can help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Dec 2015 07:47:32 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2015-12-11T07:47:32Z</dc:date>
    <item>
      <title>MWCT1001A for Auto Wireless Charging</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MWCT1001A-for-Auto-Wireless-Charging/m-p/470302#M635</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Experts&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using a MWCT1001A for Auto Wireless Charging application.&lt;/P&gt;&lt;P&gt;Refer to the datasheet, it is possible to choose internal OSC 8MHz for system clock.&lt;/P&gt;&lt;P&gt;But, how to modify the source code to disable external crystal and works well?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Dec 2015 11:38:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MWCT1001A-for-Auto-Wireless-Charging/m-p/470302#M635</guid>
      <dc:creator>kyleyang</dc:creator>
      <dc:date>2015-12-08T11:38:23Z</dc:date>
    </item>
    <item>
      <title>Re: MWCT1001A for Auto Wireless Charging</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MWCT1001A-for-Auto-Wireless-Charging/m-p/470303#M636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Kyle,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Of course, the MWCT1001A has internal 8MHz relaxation oscillator, it is the default clock in the source code, after reset, the default 8mhz relaxation oscillator clock is used. If you use internal 8MHz clock, do not use external crystal, you should set CLK_MODE bit as 1(External clock bypass mode) and set the COHL as 1(low power mode to save power) , the two pins GPIOC0/EXTAL, GPIOC1/XTAL can be configured as GPIO pins and external crystal is disabled.&lt;/P&gt;&lt;P&gt;Hope it can help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Dec 2015 07:47:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MWCT1001A-for-Auto-Wireless-Charging/m-p/470303#M636</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2015-12-11T07:47:32Z</dc:date>
    </item>
    <item>
      <title>Re: MWCT1001A for Auto Wireless Charging</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MWCT1001A-for-Auto-Wireless-Charging/m-p/470304#M637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, fix the issue already.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 13 Dec 2015 13:44:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MWCT1001A-for-Auto-Wireless-Charging/m-p/470304#M637</guid>
      <dc:creator>kyleyang</dc:creator>
      <dc:date>2015-12-13T13:44:00Z</dc:date>
    </item>
  </channel>
</rss>