<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC56F8006 - Low Frequency PWM in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8006-Low-Frequency-PWM/m-p/454912#M601</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;The general answer is of course this can be done.&amp;nbsp; However, what is the clock frequency you are running the system at?&lt;/P&gt;&lt;P&gt;It can be set to a very low frequency to save power. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;HOW to do this will depend on what else you are doing at the same time; the complete system view would help, or as much as you can share.&lt;/P&gt;&lt;P&gt;If you wish to keep such confidential, I suggest using the technical information center support available at &lt;A href="https://community.nxp.com/www.freescale.com" target="test_blank"&gt;www.freescale.com&lt;/A&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 May 2015 17:20:31 GMT</pubDate>
    <dc:creator>johnlwinters</dc:creator>
    <dc:date>2015-05-26T17:20:31Z</dc:date>
    <item>
      <title>MC56F8006 - Low Frequency PWM</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8006-Low-Frequency-PWM/m-p/454911#M600</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is possible to achieve a 10Hz frequency in the PWM module?&lt;/P&gt;&lt;P&gt;If is it possible, which are the correct settings? &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 May 2015 23:10:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8006-Low-Frequency-PWM/m-p/454911#M600</guid>
      <dc:creator>CarlosCba</dc:creator>
      <dc:date>2015-05-21T23:10:48Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F8006 - Low Frequency PWM</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8006-Low-Frequency-PWM/m-p/454912#M601</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;The general answer is of course this can be done.&amp;nbsp; However, what is the clock frequency you are running the system at?&lt;/P&gt;&lt;P&gt;It can be set to a very low frequency to save power. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;HOW to do this will depend on what else you are doing at the same time; the complete system view would help, or as much as you can share.&lt;/P&gt;&lt;P&gt;If you wish to keep such confidential, I suggest using the technical information center support available at &lt;A href="https://community.nxp.com/www.freescale.com" target="test_blank"&gt;www.freescale.com&lt;/A&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 May 2015 17:20:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8006-Low-Frequency-PWM/m-p/454912#M601</guid>
      <dc:creator>johnlwinters</dc:creator>
      <dc:date>2015-05-26T17:20:31Z</dc:date>
    </item>
  </channel>
</rss>