<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal Controllers中的主题 Re: Problems with &amp;quot;Fault Glitch Stretch Enable&amp;quot;</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Problems-with-quot-Fault-Glitch-Stretch-Enable-quot/m-p/443129#M574</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Jan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you know, the PWM_FAULTx signal is very sensitive to noise, in order to avoid the scenario&amp;nbsp; that the noise disable PWM signals unexpectedly, we design the filtering function of the fault pins.&lt;/P&gt;&lt;P&gt;If you do want to test the delay of the fault filter pin, pls note that the fault filter function uses IPBus clock, I suggest you set the PRSC bits in PWMA_SMnCTRL as 0 so that the IPBus clock can also drive the PWMA_SMnCNT. set the PWMA_SMnVAL1 as 10 or less so that the PWM frequency is high. then you can compare the delay between fault signal and disabled PWM signal.&lt;/P&gt;&lt;P&gt;Hope it can help you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Jun 2015 09:04:23 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2015-06-10T09:04:23Z</dc:date>
    <item>
      <title>Problems with "Fault Glitch Stretch Enable"</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Problems-with-quot-Fault-Glitch-Stretch-Enable-quot/m-p/443128#M573</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the MC56F82748 DSC for a PM motor controller.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In this relation I have tried to apply HW filtering of a Fault input. More specifically, I try to apply the "Fault Glitch Stretch Enable" functionality in the register PWMA_FFILTn, however it does not seem to work.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Shortly described, my problem is that no matter, how many samples I apply or which sample rate, the delay applied by the DSC between a signal at the input and PWM inhibit does not change and stays close to zero. It seems like, a change in input voltage bypasses the filter and inhibits the PWM right away, regardless of the delay defined in the register.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 1.5;"&gt;Does anyone have experience using the glitch filter?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jun 2015 16:21:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Problems-with-quot-Fault-Glitch-Stretch-Enable-quot/m-p/443128#M573</guid>
      <dc:creator>jan1</dc:creator>
      <dc:date>2015-06-09T16:21:31Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with "Fault Glitch Stretch Enable"</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Problems-with-quot-Fault-Glitch-Stretch-Enable-quot/m-p/443129#M574</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Jan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you know, the PWM_FAULTx signal is very sensitive to noise, in order to avoid the scenario&amp;nbsp; that the noise disable PWM signals unexpectedly, we design the filtering function of the fault pins.&lt;/P&gt;&lt;P&gt;If you do want to test the delay of the fault filter pin, pls note that the fault filter function uses IPBus clock, I suggest you set the PRSC bits in PWMA_SMnCTRL as 0 so that the IPBus clock can also drive the PWMA_SMnCNT. set the PWMA_SMnVAL1 as 10 or less so that the PWM frequency is high. then you can compare the delay between fault signal and disabled PWM signal.&lt;/P&gt;&lt;P&gt;Hope it can help you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2015 09:04:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Problems-with-quot-Fault-Glitch-Stretch-Enable-quot/m-p/443129#M574</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2015-06-10T09:04:23Z</dc:date>
    </item>
  </channel>
</rss>