<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal ControllersのトピックRe: 3PHASE-LV-kit: Not able to get USB com port up</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/3PHASE-LV-kit-Not-able-to-get-USB-com-port-up/m-p/423729#M529</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Ankur,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you know that there is a chip MC9S08 MCU on the power stage board, which is CDC device and can transform SCI protocol to USB so that you can use Freemaster tools to communicate.&lt;/P&gt;&lt;P&gt;I attach the driver and the code run on MC9S08, you can download the USB_SCI_driver.s19 file to MC9S08 from the J9 BDM port&amp;nbsp; on board via Multilink Universal device or BDM Multilink device from PE company.&lt;/P&gt;&lt;P&gt;The USB driver running on PC HC9S08JMxx.inf is attached.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Jun 2015 04:48:20 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2015-06-08T04:48:20Z</dc:date>
    <item>
      <title>3PHASE-LV-kit: Not able to get USB com port up</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/3PHASE-LV-kit-Not-able-to-get-USB-com-port-up/m-p/423728#M528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When i attach USB cable, "Install Device driver" always fails on Windows and no relief even if i give locations for HC9S08JMxx and usbser.sys files&lt;/P&gt;&lt;P&gt;Can you help how to make this link up. Because of this USB connection issue, not able to run any demo applications.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jun 2015 11:19:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/3PHASE-LV-kit-Not-able-to-get-USB-com-port-up/m-p/423728#M528</guid>
      <dc:creator>ankurroy</dc:creator>
      <dc:date>2015-06-03T11:19:44Z</dc:date>
    </item>
    <item>
      <title>Re: 3PHASE-LV-kit: Not able to get USB com port up</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/3PHASE-LV-kit-Not-able-to-get-USB-com-port-up/m-p/423729#M529</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Ankur,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you know that there is a chip MC9S08 MCU on the power stage board, which is CDC device and can transform SCI protocol to USB so that you can use Freemaster tools to communicate.&lt;/P&gt;&lt;P&gt;I attach the driver and the code run on MC9S08, you can download the USB_SCI_driver.s19 file to MC9S08 from the J9 BDM port&amp;nbsp; on board via Multilink Universal device or BDM Multilink device from PE company.&lt;/P&gt;&lt;P&gt;The USB driver running on PC HC9S08JMxx.inf is attached.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jun 2015 04:48:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/3PHASE-LV-kit-Not-able-to-get-USB-com-port-up/m-p/423729#M529</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2015-06-08T04:48:20Z</dc:date>
    </item>
  </channel>
</rss>