<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal Controllers中的主题 MWCT1001A: Debugging via JTAG/Once when switching from normal to fast mode?</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MWCT1001A-Debugging-via-JTAG-Once-when-switching-from-normal-to/m-p/417913#M509</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We use the WCTAutoA13 wireless charging library on a MWCT1001A to develop a wireless charging solution.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;At some point during system init the library switches from normal mode to fast mode. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This involves a soft reset by setting the SWR bit in the SIM_RSTAT register. (see Chapter 5.4.1 Sequence involving Run mode switching in the MWCT100X RM for details) &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After issuing that soft reset the debugger loses connection (JTAG state is reset when soft reset is executed) making it so I'm unable to debug the SW. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a way to use JTAG/Once debugging when a SW switches from normal mode to fast mode and a soft reset is issued? &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CW 10.6 &lt;/P&gt;&lt;P&gt;Windows XP &lt;/P&gt;&lt;P&gt;P&amp;amp;E Micro Multilink FX&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jul 2015 17:53:25 GMT</pubDate>
    <dc:creator>christianflügel</dc:creator>
    <dc:date>2015-07-16T17:53:25Z</dc:date>
    <item>
      <title>MWCT1001A: Debugging via JTAG/Once when switching from normal to fast mode?</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MWCT1001A-Debugging-via-JTAG-Once-when-switching-from-normal-to/m-p/417913#M509</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We use the WCTAutoA13 wireless charging library on a MWCT1001A to develop a wireless charging solution.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;At some point during system init the library switches from normal mode to fast mode. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This involves a soft reset by setting the SWR bit in the SIM_RSTAT register. (see Chapter 5.4.1 Sequence involving Run mode switching in the MWCT100X RM for details) &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After issuing that soft reset the debugger loses connection (JTAG state is reset when soft reset is executed) making it so I'm unable to debug the SW. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a way to use JTAG/Once debugging when a SW switches from normal mode to fast mode and a soft reset is issued? &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CW 10.6 &lt;/P&gt;&lt;P&gt;Windows XP &lt;/P&gt;&lt;P&gt;P&amp;amp;E Micro Multilink FX&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jul 2015 17:53:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MWCT1001A-Debugging-via-JTAG-Once-when-switching-from-normal-to/m-p/417913#M509</guid>
      <dc:creator>christianflügel</dc:creator>
      <dc:date>2015-07-16T17:53:25Z</dc:date>
    </item>
    <item>
      <title>Re: MWCT1001A: Debugging via JTAG/Once when switching from normal to fast mode?</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MWCT1001A-Debugging-via-JTAG-Once-when-switching-from-normal-to/m-p/417914#M510</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you using USBTAP for debugging MWCT1001A? This is a known problem that the debugger loses connection after JTAG reset. With multilink universal, we have no such problem. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fiona Kuang&lt;/P&gt;&lt;P&gt;Technical Information &amp;amp; Commercial Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Jul 2015 08:19:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MWCT1001A-Debugging-via-JTAG-Once-when-switching-from-normal-to/m-p/417914#M510</guid>
      <dc:creator>TICS_Fiona</dc:creator>
      <dc:date>2015-07-31T08:19:20Z</dc:date>
    </item>
  </channel>
</rss>