<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SC18IS604PWU No Interrupt Signal in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/SC18IS604PWU-No-Interrupt-Signal/m-p/2150792#M3805</link>
    <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am writing to request assistance regarding an issue with your &lt;STRONG&gt;SC18IS604PWU&lt;/STRONG&gt; SPI-to-I2C converter.&lt;/P&gt;&lt;P&gt;The core problem is that the converter is not asserting the interrupt signal from the I2C_INT pin, even after being properly initialized via the SPI bus. Consequently, our DSP is not triggered to initiate I2C communication.&lt;/P&gt;&lt;P&gt;I have performed the following troubleshooting steps:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;Software Verification&lt;/STRONG&gt;: I am using the exact same firmware that operates correctly on an older, functional version of our board, where the converter generates the interrupt signal as expected.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;Hardware Inspection (New Board)&lt;/STRONG&gt;:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;Continuity Check&lt;/STRONG&gt;: I have verified the continuity of all SPI and interrupt signal traces with a multimeter. All connections are sound.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;Signal Measurement&lt;/STRONG&gt;: Using an oscilloscope, I have probed the I2C_INT pin directly on the converter and observed no activity whatsoever (no falling edge).&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;Input Signals&lt;/STRONG&gt;: I have confirmed that the VCC and RESET pins of the converter are operating correctly. I have also verified that the incoming SPI signals (SCLK, MOSI, and CS) are present and correct, matching the signals on the working board.&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Since the component functions correctly on an older board with the same software, but fails on a new board despite extensive hardware verification, I suspect a potential component manufacturing issue or a subtle timing-related problem that is not immediately apparent.&lt;/P&gt;&lt;P&gt;I can provide the relevant schematics and oscilloscope captures of the working board's operation if necessary.&lt;/P&gt;&lt;P&gt;Any guidance you can provide to help resolve this issue would be greatly appreciated.&lt;/P&gt;</description>
    <pubDate>Tue, 12 Aug 2025 09:20:26 GMT</pubDate>
    <dc:creator>drormoshe</dc:creator>
    <dc:date>2025-08-12T09:20:26Z</dc:date>
    <item>
      <title>SC18IS604PWU No Interrupt Signal</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/SC18IS604PWU-No-Interrupt-Signal/m-p/2150792#M3805</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am writing to request assistance regarding an issue with your &lt;STRONG&gt;SC18IS604PWU&lt;/STRONG&gt; SPI-to-I2C converter.&lt;/P&gt;&lt;P&gt;The core problem is that the converter is not asserting the interrupt signal from the I2C_INT pin, even after being properly initialized via the SPI bus. Consequently, our DSP is not triggered to initiate I2C communication.&lt;/P&gt;&lt;P&gt;I have performed the following troubleshooting steps:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;Software Verification&lt;/STRONG&gt;: I am using the exact same firmware that operates correctly on an older, functional version of our board, where the converter generates the interrupt signal as expected.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;Hardware Inspection (New Board)&lt;/STRONG&gt;:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;Continuity Check&lt;/STRONG&gt;: I have verified the continuity of all SPI and interrupt signal traces with a multimeter. All connections are sound.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;Signal Measurement&lt;/STRONG&gt;: Using an oscilloscope, I have probed the I2C_INT pin directly on the converter and observed no activity whatsoever (no falling edge).&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;Input Signals&lt;/STRONG&gt;: I have confirmed that the VCC and RESET pins of the converter are operating correctly. I have also verified that the incoming SPI signals (SCLK, MOSI, and CS) are present and correct, matching the signals on the working board.&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Since the component functions correctly on an older board with the same software, but fails on a new board despite extensive hardware verification, I suspect a potential component manufacturing issue or a subtle timing-related problem that is not immediately apparent.&lt;/P&gt;&lt;P&gt;I can provide the relevant schematics and oscilloscope captures of the working board's operation if necessary.&lt;/P&gt;&lt;P&gt;Any guidance you can provide to help resolve this issue would be greatly appreciated.&lt;/P&gt;</description>
      <pubDate>Tue, 12 Aug 2025 09:20:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/SC18IS604PWU-No-Interrupt-Signal/m-p/2150792#M3805</guid>
      <dc:creator>drormoshe</dc:creator>
      <dc:date>2025-08-12T09:20:26Z</dc:date>
    </item>
    <item>
      <title>Re: SC18IS604PWU No Interrupt Signal</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/SC18IS604PWU-No-Interrupt-Signal/m-p/2151065#M3806</link>
      <description>&lt;P&gt;Hello drormoshe&lt;/P&gt;
&lt;P&gt;Good day!&lt;/P&gt;
&lt;P&gt;Yes please, it would be very helpful to see your schematic and capture of your communication signal and I2C_INT&lt;/P&gt;
&lt;P&gt;I will be waiting for your response&lt;/P&gt;
&lt;P&gt;Have a great day and best of luck.&lt;/P&gt;</description>
      <pubDate>Tue, 12 Aug 2025 17:56:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/SC18IS604PWU-No-Interrupt-Signal/m-p/2151065#M3806</guid>
      <dc:creator>RafaR</dc:creator>
      <dc:date>2025-08-12T17:56:47Z</dc:date>
    </item>
  </channel>
</rss>