<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can P3S0200GM be used for USB FS signals? in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Can-P3S0200GM-be-used-for-USB-FS-signals/m-p/2130621#M3792</link>
    <description>&lt;P&gt;Dear M. Havu,&lt;/P&gt;
&lt;P&gt;the&amp;nbsp;P3S0200GM&amp;nbsp;is a&amp;nbsp;2-bit bidirectional voltage-level translator and multiplexer&amp;nbsp;designed primarily for&amp;nbsp;I²C and I³C&amp;nbsp;signals. It is&amp;nbsp;not suitable for multiplexing full-speed USB signals.&lt;/P&gt;
&lt;P&gt;It does not support the USB differential signaling (D+/D-).&lt;/P&gt;
&lt;P&gt;We can recommend you&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/data-sheet/CBTL02043A_CBTL02043B.pdf" target="_self"&gt;CBTL02043A; CBTL02043B&lt;/A&gt;&amp;nbsp;2:1 mux/demux for the USB signals.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/interfaces/usb-interfaces/3-3-v-two-differential-channel-2-1-multiplexer-demultiplexer-switch:CBTL02043A_CBTL02043B?fpsp=1#documentation" target="_blank"&gt;https://www.nxp.com/products/interfaces/usb-interfaces/3-3-v-two-differential-channel-2-1-multiplexer-demultiplexer-switch:CBTL02043A_CBTL02043B?fpsp=1#documentation&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
    <pubDate>Wed, 09 Jul 2025 06:07:04 GMT</pubDate>
    <dc:creator>JozefKozon</dc:creator>
    <dc:date>2025-07-09T06:07:04Z</dc:date>
    <item>
      <title>Can P3S0200GM be used for USB FS signals?</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Can-P3S0200GM-be-used-for-USB-FS-signals/m-p/2130267#M3791</link>
      <description>&lt;P&gt;Can P3S0200GM be used for multiplexing full-speed USB signals? We already use it elsewhere in the design, so it would be convenient to use the same part, if possible.&lt;/P&gt;</description>
      <pubDate>Tue, 08 Jul 2025 15:50:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Can-P3S0200GM-be-used-for-USB-FS-signals/m-p/2130267#M3791</guid>
      <dc:creator>mhavu</dc:creator>
      <dc:date>2025-07-08T15:50:34Z</dc:date>
    </item>
    <item>
      <title>Re: Can P3S0200GM be used for USB FS signals?</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Can-P3S0200GM-be-used-for-USB-FS-signals/m-p/2130621#M3792</link>
      <description>&lt;P&gt;Dear M. Havu,&lt;/P&gt;
&lt;P&gt;the&amp;nbsp;P3S0200GM&amp;nbsp;is a&amp;nbsp;2-bit bidirectional voltage-level translator and multiplexer&amp;nbsp;designed primarily for&amp;nbsp;I²C and I³C&amp;nbsp;signals. It is&amp;nbsp;not suitable for multiplexing full-speed USB signals.&lt;/P&gt;
&lt;P&gt;It does not support the USB differential signaling (D+/D-).&lt;/P&gt;
&lt;P&gt;We can recommend you&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/data-sheet/CBTL02043A_CBTL02043B.pdf" target="_self"&gt;CBTL02043A; CBTL02043B&lt;/A&gt;&amp;nbsp;2:1 mux/demux for the USB signals.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/interfaces/usb-interfaces/3-3-v-two-differential-channel-2-1-multiplexer-demultiplexer-switch:CBTL02043A_CBTL02043B?fpsp=1#documentation" target="_blank"&gt;https://www.nxp.com/products/interfaces/usb-interfaces/3-3-v-two-differential-channel-2-1-multiplexer-demultiplexer-switch:CBTL02043A_CBTL02043B?fpsp=1#documentation&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jul 2025 06:07:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Can-P3S0200GM-be-used-for-USB-FS-signals/m-p/2130621#M3792</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2025-07-09T06:07:04Z</dc:date>
    </item>
  </channel>
</rss>