<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC56F83789:Controller stops at Entry point of interrupt vector table. in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F83789-Controller-stops-at-Entry-point-of-interrupt-vector/m-p/1995058#M3597</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I guess that you have configured the GPIO port interrupt enabled, so the GPIO pin rising or falling edge triggers an interrupt, but you do not have ISR for the port.&lt;/P&gt;
&lt;P&gt;Can you tell us which GPIO pin makes the core to stop at the entry point? is it convenient for&amp;nbsp; you to post the code?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Fri, 15 Nov 2024 02:23:24 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2024-11-15T02:23:24Z</dc:date>
    <item>
      <title>MC56F83789:Controller stops at Entry point of interrupt vector table.</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F83789-Controller-stops-at-Entry-point-of-interrupt-vector/m-p/1994263#M3593</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;While I was working with one code, the normally it operates well, but when a Gpio input is given the program stops at entry poin of interrupt vector table. Please see the screenshot.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please let me know the reason for the same or the steps to debug.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26034"&gt;@xiangjun_rong&lt;/a&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Nov 2024 05:22:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F83789-Controller-stops-at-Entry-point-of-interrupt-vector/m-p/1994263#M3593</guid>
      <dc:creator>Aman786</dc:creator>
      <dc:date>2024-11-14T05:22:46Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F83789:Controller stops at Entry point of interrupt vector table.</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F83789-Controller-stops-at-Entry-point-of-interrupt-vector/m-p/1995058#M3597</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I guess that you have configured the GPIO port interrupt enabled, so the GPIO pin rising or falling edge triggers an interrupt, but you do not have ISR for the port.&lt;/P&gt;
&lt;P&gt;Can you tell us which GPIO pin makes the core to stop at the entry point? is it convenient for&amp;nbsp; you to post the code?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Fri, 15 Nov 2024 02:23:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F83789-Controller-stops-at-Entry-point-of-interrupt-vector/m-p/1995058#M3597</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-11-15T02:23:24Z</dc:date>
    </item>
  </channel>
</rss>