<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal ControllersのトピックRe: not able to connect to MC56F8367 with CodeWarrior USB TAP Rev E</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/not-able-to-connect-to-MC56F8367-with-CodeWarrior-USB-TAP-Rev-E/m-p/1971819#M3580</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I am sure that the CodeWarrior for MCU tools has not any problem run on PC with windows 10.&lt;/P&gt;
&lt;P&gt;From hardware perspective, pls pay attention to the pin 1 of 14 pin JTAG connector on your PCB, the&amp;nbsp; red cable of 14 flat cable for USBTAP device is pin1.&lt;/P&gt;
&lt;P&gt;I have not the other idea why you can not connect, maybe the USBTAP device has issue.&lt;/P&gt;
&lt;P&gt;As an alternative, you can use Multilink Universal device with CodeWarrior for MCU tools to download/debug which is third party device .&lt;/P&gt;
&lt;P&gt;&lt;A href="http://www.pemicro.com" target="_blank"&gt;www.pemicro.com&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 11 Oct 2024 03:26:07 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2024-10-11T03:26:07Z</dc:date>
    <item>
      <title>not able to connect to MC56F8367 with CodeWarrior USB TAP Rev E</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/not-able-to-connect-to-MC56F8367-with-CodeWarrior-USB-TAP-Rev-E/m-p/1970887#M3573</link>
      <description>&lt;P&gt;I'm not able to connect to MC56F8367 with CodeWarrior USB TAP Rev E - ONCE. I'm using CodeWarrior for MCU&lt;BR /&gt;Version: 10.6.4&lt;BR /&gt;Build Id:150416&lt;/P&gt;&lt;P&gt;Error launching Motion_56F8367_FLASH_LDM_FSL USB TAP&lt;BR /&gt;Bad arguments passed to function&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But I'm able to connect using CodeWarrior USB TAP Rev F - ONCE.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jeevankumar_0-1728532400645.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/303890iC6356B202BED6665/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jeevankumar_0-1728532400645.png" alt="jeevankumar_0-1728532400645.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;jeevankumar_0-1728532400645.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Oct 2024 03:54:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/not-able-to-connect-to-MC56F8367-with-CodeWarrior-USB-TAP-Rev-E/m-p/1970887#M3573</guid>
      <dc:creator>jeevankumar</dc:creator>
      <dc:date>2024-10-10T03:54:07Z</dc:date>
    </item>
    <item>
      <title>Re: not able to connect to MC56F8367 with CodeWarrior USB TAP Rev E</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/not-able-to-connect-to-MC56F8367-with-CodeWarrior-USB-TAP-Rev-E/m-p/1971819#M3580</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I am sure that the CodeWarrior for MCU tools has not any problem run on PC with windows 10.&lt;/P&gt;
&lt;P&gt;From hardware perspective, pls pay attention to the pin 1 of 14 pin JTAG connector on your PCB, the&amp;nbsp; red cable of 14 flat cable for USBTAP device is pin1.&lt;/P&gt;
&lt;P&gt;I have not the other idea why you can not connect, maybe the USBTAP device has issue.&lt;/P&gt;
&lt;P&gt;As an alternative, you can use Multilink Universal device with CodeWarrior for MCU tools to download/debug which is third party device .&lt;/P&gt;
&lt;P&gt;&lt;A href="http://www.pemicro.com" target="_blank"&gt;www.pemicro.com&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Oct 2024 03:26:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/not-able-to-connect-to-MC56F8367-with-CodeWarrior-USB-TAP-Rev-E/m-p/1971819#M3580</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-10-11T03:26:07Z</dc:date>
    </item>
    <item>
      <title>Re: not able to connect to MC56F8367 with CodeWarrior USB TAP Rev E</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/not-able-to-connect-to-MC56F8367-with-CodeWarrior-USB-TAP-Rev-E/m-p/1972064#M3582</link>
      <description>Hi XiangJun , Thanks for reply.&lt;BR /&gt;&lt;BR /&gt;Yes I made sure Pin connections are correct.&lt;BR /&gt;Basically I have two CW USB TAP devices - Rev E and REV F. I'm able to connect with Rev F without any issue. But not able to connect with Rev E.&lt;BR /&gt;Any idea why I'm not able to connect using Rev E device? Am I missing anything?</description>
      <pubDate>Fri, 11 Oct 2024 09:29:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/not-able-to-connect-to-MC56F8367-with-CodeWarrior-USB-TAP-Rev-E/m-p/1972064#M3582</guid>
      <dc:creator>jeevankumar</dc:creator>
      <dc:date>2024-10-11T09:29:45Z</dc:date>
    </item>
    <item>
      <title>Re: not able to connect to MC56F8367 with CodeWarrior USB TAP Rev E</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/not-able-to-connect-to-MC56F8367-with-CodeWarrior-USB-TAP-Rev-E/m-p/1972906#M3584</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;You have two USBTAP devices, when you download/debug MC56F8367, one works fine, another does not work, so I suppose that the second USBTAP device maybe break down.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 14 Oct 2024 02:30:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/not-able-to-connect-to-MC56F8367-with-CodeWarrior-USB-TAP-Rev-E/m-p/1972906#M3584</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-10-14T02:30:36Z</dc:date>
    </item>
  </channel>
</rss>