<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How can I use VCPU/IPPU memory when woking with NLM project/LCF on LA9310 RDB in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/How-can-I-use-VCPU-IPPU-memory-when-woking-with-NLM-project-LCF/m-p/1948745#M3550</link>
    <description>&lt;P&gt;Hi experts,&lt;BR /&gt;I'm new working on LA9310 Network listening module (NLM) 5g_nlm_vspa_isc project.&lt;/P&gt;&lt;P&gt;I use la9310_nmm_app.lcf but with VSPA main.c is a example code created from codewarrior 9310 project.&lt;/P&gt;&lt;P&gt;I modified main.c to make run shival OK (mailbox to/from shival OK).&lt;/P&gt;&lt;P&gt;But I have two memory issue when I attach VSPA in debug mode:&lt;BR /&gt;1. LA9310 claims 32KB memory space for VCPU and IPPU, but codewarrior variable window in debug mode shows 16KB memory space only? I can use 16KB only?&lt;/P&gt;&lt;P&gt;2. I use memset to clean VCPU 16KB memory, also codewarrior window show VCPU memory not cleaned. but VSPA dump file via sim_dram_save shows memory is cleaned. I am not sure VCPU is cleaned or not.&lt;/P&gt;&lt;P&gt;Are there any specific consideration when working with LA9310 NLM VSPA memory space&lt;/P&gt;&lt;P&gt;I would greatly appreciate any advise. Thanks&lt;/P&gt;</description>
    <pubDate>Fri, 06 Sep 2024 05:46:49 GMT</pubDate>
    <dc:creator>jerry017</dc:creator>
    <dc:date>2024-09-06T05:46:49Z</dc:date>
    <item>
      <title>How can I use VCPU/IPPU memory when woking with NLM project/LCF on LA9310 RDB</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/How-can-I-use-VCPU-IPPU-memory-when-woking-with-NLM-project-LCF/m-p/1948745#M3550</link>
      <description>&lt;P&gt;Hi experts,&lt;BR /&gt;I'm new working on LA9310 Network listening module (NLM) 5g_nlm_vspa_isc project.&lt;/P&gt;&lt;P&gt;I use la9310_nmm_app.lcf but with VSPA main.c is a example code created from codewarrior 9310 project.&lt;/P&gt;&lt;P&gt;I modified main.c to make run shival OK (mailbox to/from shival OK).&lt;/P&gt;&lt;P&gt;But I have two memory issue when I attach VSPA in debug mode:&lt;BR /&gt;1. LA9310 claims 32KB memory space for VCPU and IPPU, but codewarrior variable window in debug mode shows 16KB memory space only? I can use 16KB only?&lt;/P&gt;&lt;P&gt;2. I use memset to clean VCPU 16KB memory, also codewarrior window show VCPU memory not cleaned. but VSPA dump file via sim_dram_save shows memory is cleaned. I am not sure VCPU is cleaned or not.&lt;/P&gt;&lt;P&gt;Are there any specific consideration when working with LA9310 NLM VSPA memory space&lt;/P&gt;&lt;P&gt;I would greatly appreciate any advise. Thanks&lt;/P&gt;</description>
      <pubDate>Fri, 06 Sep 2024 05:46:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/How-can-I-use-VCPU-IPPU-memory-when-woking-with-NLM-project-LCF/m-p/1948745#M3550</guid>
      <dc:creator>jerry017</dc:creator>
      <dc:date>2024-09-06T05:46:49Z</dc:date>
    </item>
  </channel>
</rss>