<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PCA9698DGG maximum toggling frequency in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9698DGG-maximum-toggling-frequency/m-p/1921194#M3455</link>
    <description>&lt;P&gt;Dear team,&lt;/P&gt;&lt;P&gt;We are using PCA9698DGG in our design, we are planning to use the mentioned component to drive a clock frequency of about 30 Mhz and receive the same.Kindly provide the max. &amp;amp; min recommended Tx and Rx frequency limit for the mentioned component.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Blessing Selvakumar,&lt;BR /&gt;Hardware Design Engineer.&lt;/P&gt;</description>
    <pubDate>Wed, 31 Jul 2024 05:33:45 GMT</pubDate>
    <dc:creator>Blessing</dc:creator>
    <dc:date>2024-07-31T05:33:45Z</dc:date>
    <item>
      <title>PCA9698DGG maximum toggling frequency</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9698DGG-maximum-toggling-frequency/m-p/1921194#M3455</link>
      <description>&lt;P&gt;Dear team,&lt;/P&gt;&lt;P&gt;We are using PCA9698DGG in our design, we are planning to use the mentioned component to drive a clock frequency of about 30 Mhz and receive the same.Kindly provide the max. &amp;amp; min recommended Tx and Rx frequency limit for the mentioned component.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Blessing Selvakumar,&lt;BR /&gt;Hardware Design Engineer.&lt;/P&gt;</description>
      <pubDate>Wed, 31 Jul 2024 05:33:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9698DGG-maximum-toggling-frequency/m-p/1921194#M3455</guid>
      <dc:creator>Blessing</dc:creator>
      <dc:date>2024-07-31T05:33:45Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9698DGG maximum toggling frequency</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9698DGG-maximum-toggling-frequency/m-p/1921270#M3456</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Do you mean to use PCA9698 generate 30MHz PWM/clock signal?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 31 Jul 2024 06:47:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9698DGG-maximum-toggling-frequency/m-p/1921270#M3456</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2024-07-31T06:47:39Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9698DGG maximum toggling frequency</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9698DGG-maximum-toggling-frequency/m-p/1922459#M3457</link>
      <description>&lt;P&gt;Hi Guoweisun,&lt;/P&gt;&lt;P&gt;Yes,I need to know whether PCA9698 will be able to generate a toggling data / clock at frequency &amp;lt;30 Mhz and able to receive the same if provided as input.&lt;/P&gt;</description>
      <pubDate>Thu, 01 Aug 2024 04:08:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9698DGG-maximum-toggling-frequency/m-p/1922459#M3457</guid>
      <dc:creator>Blessing</dc:creator>
      <dc:date>2024-08-01T04:08:32Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9698DGG maximum toggling frequency</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9698DGG-maximum-toggling-frequency/m-p/1926797#M3486</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;30MHZ is not possible for this part,the IIC supported speed maximum is 1MHZ.&lt;/P&gt;</description>
      <pubDate>Wed, 07 Aug 2024 01:18:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9698DGG-maximum-toggling-frequency/m-p/1926797#M3486</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2024-08-07T01:18:45Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9698DGG maximum toggling frequency</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9698DGG-maximum-toggling-frequency/m-p/1928799#M3490</link>
      <description>&lt;P&gt;Thank you for helping people get the information they need. Great stuff as usual. Keep up the great work!!!&amp;nbsp;&lt;A href="https://www.ny-stateofhealth.com" target="_self"&gt;NYStateofHealth&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 09 Aug 2024 04:32:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9698DGG-maximum-toggling-frequency/m-p/1928799#M3490</guid>
      <dc:creator>jennie258fitz</dc:creator>
      <dc:date>2024-08-09T04:32:16Z</dc:date>
    </item>
  </channel>
</rss>