<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal Controllers中的主题 TJA1020's RXD does not apear.</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/TJA1020-s-RXD-does-not-apear/m-p/1777901#M2893</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hello.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am developing a LIN master board using TJA1020.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In the case of TX, it signals normally and the slave also operates normally.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The problem is that when ID values are sent to receive responses, the response from the slave does not come to RX.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When analyzing the signal of the LIN line, the slave responds normally.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;However, there is no signal from the RX pin of the TJA1020.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Please let me know which part I missed.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 20 Dec 2023 23:31:41 GMT</pubDate>
    <dc:creator>Miri</dc:creator>
    <dc:date>2023-12-20T23:31:41Z</dc:date>
    <item>
      <title>TJA1020's RXD does not apear.</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/TJA1020-s-RXD-does-not-apear/m-p/1777901#M2893</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am developing a LIN master board using TJA1020.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In the case of TX, it signals normally and the slave also operates normally.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The problem is that when ID values are sent to receive responses, the response from the slave does not come to RX.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When analyzing the signal of the LIN line, the slave responds normally.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;However, there is no signal from the RX pin of the TJA1020.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Please let me know which part I missed.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Dec 2023 23:31:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/TJA1020-s-RXD-does-not-apear/m-p/1777901#M2893</guid>
      <dc:creator>Miri</dc:creator>
      <dc:date>2023-12-20T23:31:41Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1020's RXD does not apear.</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/TJA1020-s-RXD-does-not-apear/m-p/1778542#M2894</link>
      <description>&lt;P&gt;Hello Miri,&lt;/P&gt;
&lt;P&gt;Please double check that the TJA1020 is in normal slope mode:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture.JPG" style="width: 379px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/255471i3600706D4F72C126/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture.JPG" alt="Capture.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR, Tomas&lt;/P&gt;</description>
      <pubDate>Thu, 21 Dec 2023 08:27:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/TJA1020-s-RXD-does-not-apear/m-p/1778542#M2894</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2023-12-21T08:27:07Z</dc:date>
    </item>
  </channel>
</rss>