<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal ControllersのトピックRe: Problem writing code on the MC56F847 DSP</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Problem-writing-code-on-the-MC56F847-DSP/m-p/1728406#M2834</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Can you tell us the part number you are using? There is not MC56F847, maybe it is MC56F84789 or something like that&lt;/P&gt;
&lt;P&gt;what is the tools you are using for example CodeWarrior for MVU ver11.x?&lt;/P&gt;
&lt;P&gt;Do you use USBTAP or Multilink Universal device?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 25 Sep 2023 01:34:29 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2023-09-25T01:34:29Z</dc:date>
    <item>
      <title>Problem writing code on the MC56F847 DSP</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Problem-writing-code-on-the-MC56F847-DSP/m-p/1728135#M2833</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello, I'm having the following problem running the code on the DSP:&amp;nbsp;Error: Couldn't write applet to target. Can not read target memory at location: 0x0000000000000000.Please make sure that the chip selects are properly configured.&lt;BR /&gt;The CWPP response code is: CCSProtocolPlugin : CCS: Core not responding.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;I'm using the correct settings for the chip because I've been using the same code for weeks, this problem started to happen out of nowhere.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 22 Sep 2023 15:34:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Problem-writing-code-on-the-MC56F847-DSP/m-p/1728135#M2833</guid>
      <dc:creator>Michell</dc:creator>
      <dc:date>2023-09-22T15:34:51Z</dc:date>
    </item>
    <item>
      <title>Re: Problem writing code on the MC56F847 DSP</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Problem-writing-code-on-the-MC56F847-DSP/m-p/1728406#M2834</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Can you tell us the part number you are using? There is not MC56F847, maybe it is MC56F84789 or something like that&lt;/P&gt;
&lt;P&gt;what is the tools you are using for example CodeWarrior for MVU ver11.x?&lt;/P&gt;
&lt;P&gt;Do you use USBTAP or Multilink Universal device?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 25 Sep 2023 01:34:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Problem-writing-code-on-the-MC56F847-DSP/m-p/1728406#M2834</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-09-25T01:34:29Z</dc:date>
    </item>
  </channel>
</rss>