<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal Controllers中的主题 Re: MC56F8355 start up</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8355-start-up/m-p/1723804#M2822</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the temperature is 25°C, it's OK.&lt;/P&gt;&lt;P&gt;If the temperature is 10°C or 50°C, it's not OK.&lt;/P&gt;&lt;P&gt;I changed crystal by a ceramic resonator 8MHz and I can start the µcontroller at 10 and 50°C.&lt;/P&gt;&lt;P&gt;Is it necessary to change the bit&amp;nbsp; register COHL which is at&amp;nbsp; 1.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Christophe&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 15 Sep 2023 09:15:06 GMT</pubDate>
    <dc:creator>christophe_c</dc:creator>
    <dc:date>2023-09-15T09:15:06Z</dc:date>
    <item>
      <title>MC56F8355 start up</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8355-start-up/m-p/1723151#M2818</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I use an MC56F8355 and it doesn't start when I heat it.&lt;/P&gt;&lt;P&gt;The RESET signal is OK but the RSTO signal stayes at 0.&lt;/P&gt;&lt;P&gt;Thank you for your help&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Christophe&lt;/P&gt;</description>
      <pubDate>Thu, 14 Sep 2023 12:46:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8355-start-up/m-p/1723151#M2818</guid>
      <dc:creator>christophe_c</dc:creator>
      <dc:date>2023-09-14T12:46:42Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F8355 start up</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8355-start-up/m-p/1723542#M2820</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suppose that the MC56F8355 can run if you don't heat it.&lt;/P&gt;
&lt;P&gt;This is the ambient temperature range the MC56F8355 can work.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1694747827480.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/241123i7CD7AC12671F06A9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1694747827480.png" alt="xiangjun_rong_0-1694747827480.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Sep 2023 03:18:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8355-start-up/m-p/1723542#M2820</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-09-15T03:18:19Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F8355 start up</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8355-start-up/m-p/1723804#M2822</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the temperature is 25°C, it's OK.&lt;/P&gt;&lt;P&gt;If the temperature is 10°C or 50°C, it's not OK.&lt;/P&gt;&lt;P&gt;I changed crystal by a ceramic resonator 8MHz and I can start the µcontroller at 10 and 50°C.&lt;/P&gt;&lt;P&gt;Is it necessary to change the bit&amp;nbsp; register COHL which is at&amp;nbsp; 1.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Christophe&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Sep 2023 09:15:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8355-start-up/m-p/1723804#M2822</guid>
      <dc:creator>christophe_c</dc:creator>
      <dc:date>2023-09-15T09:15:06Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F8355 start up</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8355-start-up/m-p/1724533#M2826</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;If you use 8MHz ceramic resonator, I suppose the COHL bit should be cleared.&lt;/P&gt;
&lt;P&gt;Pls refer to section 5.11.5 Oscillator Control Register w/o Relaxation Oscillator (OSCTL) in MC56F8300UM.pdf&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1695021726375.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/241379i8FAAA49AD87BF5D4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1695021726375.png" alt="xiangjun_rong_0-1695021726375.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 18 Sep 2023 07:25:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8355-start-up/m-p/1724533#M2826</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-09-18T07:25:08Z</dc:date>
    </item>
  </channel>
</rss>