<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal Controllersのトピックmingw errors while building a project</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/mingw-errors-while-building-a-project/m-p/1677761#M2751</link>
    <description>&lt;P&gt;We are using MC56F83783 controller, I installed the SDK for the controller as given.&lt;/P&gt;&lt;P&gt;After developing the code and building it, it shows some errors. The errors as follows:&lt;/P&gt;&lt;P&gt;Description Resource Path Location Type&lt;BR /&gt;mingw32-make: *** [freemaster/freemaster_appcmd_c.obj] Error 1 project1 C/C++ Problem&lt;BR /&gt;mingw32-make: *** [source/main_c.obj] Error 1 project1 C/C++ Problem&lt;BR /&gt;mingw32-make: *** [startup/Flash_config_c.obj] Error 1 project1 C/C++ Problem&lt;BR /&gt;mingw32-make: *** [startup/MC56F83783_Vectors_c.obj] Error 1 project1 C/C++ Problem&lt;BR /&gt;mingw32-make: *** Waiting for unfinished jobs.... project1 C/C++ Problem&lt;BR /&gt;mingw32-make: *** [utilities/fsl_assert_min_c.obj] Error 1 project1 C/C++ Problem&lt;BR /&gt;Specified file 'folder/project1/board' not found Operating system error: The system cannot find the path specified. project1 C/C++ Problem&lt;/P&gt;</description>
    <pubDate>Wed, 28 Jun 2023 10:02:37 GMT</pubDate>
    <dc:creator>Surya001</dc:creator>
    <dc:date>2023-06-28T10:02:37Z</dc:date>
    <item>
      <title>mingw errors while building a project</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/mingw-errors-while-building-a-project/m-p/1677761#M2751</link>
      <description>&lt;P&gt;We are using MC56F83783 controller, I installed the SDK for the controller as given.&lt;/P&gt;&lt;P&gt;After developing the code and building it, it shows some errors. The errors as follows:&lt;/P&gt;&lt;P&gt;Description Resource Path Location Type&lt;BR /&gt;mingw32-make: *** [freemaster/freemaster_appcmd_c.obj] Error 1 project1 C/C++ Problem&lt;BR /&gt;mingw32-make: *** [source/main_c.obj] Error 1 project1 C/C++ Problem&lt;BR /&gt;mingw32-make: *** [startup/Flash_config_c.obj] Error 1 project1 C/C++ Problem&lt;BR /&gt;mingw32-make: *** [startup/MC56F83783_Vectors_c.obj] Error 1 project1 C/C++ Problem&lt;BR /&gt;mingw32-make: *** Waiting for unfinished jobs.... project1 C/C++ Problem&lt;BR /&gt;mingw32-make: *** [utilities/fsl_assert_min_c.obj] Error 1 project1 C/C++ Problem&lt;BR /&gt;Specified file 'folder/project1/board' not found Operating system error: The system cannot find the path specified. project1 C/C++ Problem&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jun 2023 10:02:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/mingw-errors-while-building-a-project/m-p/1677761#M2751</guid>
      <dc:creator>Surya001</dc:creator>
      <dc:date>2023-06-28T10:02:37Z</dc:date>
    </item>
    <item>
      <title>Re: mingw errors while building a project</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/mingw-errors-while-building-a-project/m-p/1678211#M2752</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suggest you load the example button_toggle_led from the directory in SDK package&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;C:\DriveE\56F83xxxExampleCode\SDK_2_7_3_MC56F83000-EVK_D\boards\evkmc56f83000\driver_examples\gpio&lt;/P&gt;
&lt;P&gt;Then try to compile/debug&lt;/P&gt;
&lt;P&gt;For the error of your application code, pls upload the project if you can not proceed for the error.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Xiangjun Rong&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jun 2023 02:03:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/mingw-errors-while-building-a-project/m-p/1678211#M2752</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-06-29T02:03:33Z</dc:date>
    </item>
  </channel>
</rss>