<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: [MWCT2013]PWM Control in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MWCT2013-PWM-Control/m-p/1671016#M2743</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Pls refer to the code, which can be used for the MWCT2013 I suppose&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Fri, 16 Jun 2023 09:17:35 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2023-06-16T09:17:35Z</dc:date>
    <item>
      <title>[MWCT2013]PWM Control</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MWCT2013-PWM-Control/m-p/1670649#M2739</link>
      <description>&lt;P&gt;Dear NXP,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could anyone provide about the PWM initial and control code for pin 45, 46, 51?&lt;/P&gt;&lt;P&gt;I have to control each pin to output the PWM function individually.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thnak you.&lt;/P&gt;</description>
      <pubDate>Fri, 16 Jun 2023 00:44:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MWCT2013-PWM-Control/m-p/1670649#M2739</guid>
      <dc:creator>RichardT</dc:creator>
      <dc:date>2023-06-16T00:44:14Z</dc:date>
    </item>
    <item>
      <title>Re: [MWCT2013]PWM Control</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MWCT2013-PWM-Control/m-p/1670862#M2741</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As you know that the MWCT2013 has application code for wireless charging, so you have to check if the application code has used the pin pin 45, 46 and 51. If the three pins are not used, you can develop code to use them.&lt;/P&gt;
&lt;P&gt;This link has eFlexPWM application code, pls refer to it.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Digital-Signal-Controllers/Two-or-more-eFlexPWM-synchronization-for-KV4x-KV5x-MC56F84xxx/ta-p/1128526" target="_blank"&gt;https://community.nxp.com/t5/Digital-Signal-Controllers/Two-or-more-eFlexPWM-synchronization-for-KV4x-KV5x-MC56F84xxx/ta-p/1128526&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Fri, 16 Jun 2023 06:58:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MWCT2013-PWM-Control/m-p/1670862#M2741</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-06-16T06:58:11Z</dc:date>
    </item>
    <item>
      <title>Re: [MWCT2013]PWM Control</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MWCT2013-PWM-Control/m-p/1670957#M2742</link>
      <description>&lt;P&gt;Dear&amp;nbsp;&lt;SPAN&gt;XiangJun,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;unfortunately, it did not work properly after I read this document.&lt;/P&gt;&lt;P&gt;I still want to have sample code for MWCT2013.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Fri, 16 Jun 2023 08:28:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MWCT2013-PWM-Control/m-p/1670957#M2742</guid>
      <dc:creator>RichardT</dc:creator>
      <dc:date>2023-06-16T08:28:31Z</dc:date>
    </item>
    <item>
      <title>Re: [MWCT2013]PWM Control</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MWCT2013-PWM-Control/m-p/1671016#M2743</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Pls refer to the code, which can be used for the MWCT2013 I suppose&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Fri, 16 Jun 2023 09:17:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MWCT2013-PWM-Control/m-p/1671016#M2743</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-06-16T09:17:35Z</dc:date>
    </item>
  </channel>
</rss>