<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC56F84789 :PROBLEMS WITH PWMA REGISTERS AND PWMB FAULT3  FUNCTION ? in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F84789-PROBLEMS-WITH-PWMA-REGISTERS-AND-PWMB-FAULT3-FUNCTION/m-p/359281#M274</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,ZeLiang,&lt;/P&gt;&lt;P&gt;The fault pin is very sensitive to external noise, I suggest you use the Fault filter function, which can filter the noise on the Faultx pin. for detailed information, pls refer to section&amp;nbsp; 29.2.45 Fault Filter Register (PWMB_FFILTn) in the reference manual of MC56F847xx. Secondly, I suggest you do not have the fault pin float, the fault pin should be driven by external source.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Nov 2014 08:58:13 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2014-11-21T08:58:13Z</dc:date>
    <item>
      <title>MC56F84789 :PROBLEMS WITH PWMA REGISTERS AND PWMB FAULT3  FUNCTION ?</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F84789-PROBLEMS-WITH-PWMA-REGISTERS-AND-PWMB-FAULT3-FUNCTION/m-p/359280#M273</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone ! I don't understand why the PWMA_FCTRL1 and PWMA_FCTRL20 REGISTERS has the &lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/120037iDF4554E32C6A17F3/image-size/large?v=v2&amp;amp;px=999" title="16800_16800.jpg" alt="16800_16800.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/47428iDA8890C80B03D04D/image-size/large?v=v2&amp;amp;px=999" title="RT({K`4(GY8YFD@V671G_PY.jpg" alt="RT({K`4(GY8YFD@V671G_PY.jpg" /&gt;&lt;/span&gt;same address though i don't configure them for the moment.And when i enable any of&amp;nbsp; PWMB channel's&amp;nbsp; IPBUS clock , there is a fault flag set in the&amp;nbsp; PWMB_FSTS0 register anyway. There isn't having any fault&amp;nbsp; in the fault input pin . Can anybody can give some help ?&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/120038i9B8810C95EB5ED61/image-size/large?v=v2&amp;amp;px=999" title="16805_16805.jpg" alt="16805_16805.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/47429i7CDEDEF13981B70B/image-size/large?v=v2&amp;amp;px=999" title="RZ0_~@WA_]DP$UXA985N5B5.jpg" alt="RZ0_~@WA_]DP$UXA985N5B5.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Nov 2014 06:20:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F84789-PROBLEMS-WITH-PWMA-REGISTERS-AND-PWMB-FAULT3-FUNCTION/m-p/359280#M273</guid>
      <dc:creator>zhangzeliang</dc:creator>
      <dc:date>2014-11-21T06:20:16Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F84789 :PROBLEMS WITH PWMA REGISTERS AND PWMB FAULT3  FUNCTION ?</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F84789-PROBLEMS-WITH-PWMA-REGISTERS-AND-PWMB-FAULT3-FUNCTION/m-p/359281#M274</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,ZeLiang,&lt;/P&gt;&lt;P&gt;The fault pin is very sensitive to external noise, I suggest you use the Fault filter function, which can filter the noise on the Faultx pin. for detailed information, pls refer to section&amp;nbsp; 29.2.45 Fault Filter Register (PWMB_FFILTn) in the reference manual of MC56F847xx. Secondly, I suggest you do not have the fault pin float, the fault pin should be driven by external source.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Nov 2014 08:58:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F84789-PROBLEMS-WITH-PWMA-REGISTERS-AND-PWMB-FAULT3-FUNCTION/m-p/359281#M274</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2014-11-21T08:58:13Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F84789 :PROBLEMS WITH PWMA REGISTERS AND PWMB FAULT3  FUNCTION ?</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F84789-PROBLEMS-WITH-PWMA-REGISTERS-AND-PWMB-FAULT3-FUNCTION/m-p/359282#M275</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks very much&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 22 Nov 2014 00:05:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F84789-PROBLEMS-WITH-PWMA-REGISTERS-AND-PWMB-FAULT3-FUNCTION/m-p/359282#M275</guid>
      <dc:creator>zhangzeliang</dc:creator>
      <dc:date>2014-11-22T00:05:24Z</dc:date>
    </item>
  </channel>
</rss>