<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal Controllersのトピック56F837xx ref. design</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/56F837xx-ref-design/m-p/1594662#M2667</link>
    <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;Anyone can help me with ref. design for the 56f837xx chip? I want to see a sample code of using the sci with cw11. I am so used to old processor expert that I am a little lost without this feature. I want to see a sample which define sci buffers, and functions to use them.&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the firmware source code of the 56F83000-evk is available, it might help too.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Tue, 07 Feb 2023 10:49:06 GMT</pubDate>
    <dc:creator>Ben</dc:creator>
    <dc:date>2023-02-07T10:49:06Z</dc:date>
    <item>
      <title>56F837xx ref. design</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/56F837xx-ref-design/m-p/1594662#M2667</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;Anyone can help me with ref. design for the 56f837xx chip? I want to see a sample code of using the sci with cw11. I am so used to old processor expert that I am a little lost without this feature. I want to see a sample which define sci buffers, and functions to use them.&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the firmware source code of the 56F83000-evk is available, it might help too.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 07 Feb 2023 10:49:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/56F837xx-ref-design/m-p/1594662#M2667</guid>
      <dc:creator>Ben</dc:creator>
      <dc:date>2023-02-07T10:49:06Z</dc:date>
    </item>
    <item>
      <title>Re: 56F837xx ref. design</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/56F837xx-ref-design/m-p/1595171#M2669</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;For the MC56F83xxx, the PE(processor expert) tools is no longer supported, but the SDK package is supported, the SDK package provides a lot of example of peripherals including sci, pls download SDK package from the link:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://mcuxpresso.nxp.com/en/welcome" target="_blank" rel="noopener"&gt;https://mcuxpresso.nxp.com/en/welcome&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BTW, the SDK package is run on CodeWarrior for MCU ver11.x, you have to use Multilink Universal device from PE to download/debug.&lt;/P&gt;
&lt;P&gt;&lt;A href="http://www.pemicro.com" target="_blank"&gt;www.pemicro.com&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Wed, 08 Feb 2023 03:02:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/56F837xx-ref-design/m-p/1595171#M2669</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-02-08T03:02:15Z</dc:date>
    </item>
    <item>
      <title>Re: 56F837xx ref. design</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/56F837xx-ref-design/m-p/1596346#M2671</link>
      <description>&lt;P&gt;Thank you for the fast answer. generally, I am moving an old project firmware from 56F8367 to 56F83783. The demo programs in the SDK show each feature separately, but each written in a different way. It will help me to see the overall flow to understand activity with the xpresso fsl files instead of the PE files.&lt;/P&gt;&lt;P&gt;Therefore I think that if you can send me the firmware which installed on the 56f83000-evk board, it will help. Any additional tip how to make this transformation easy will be appreciated.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Benn&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 09 Feb 2023 07:55:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/56F837xx-ref-design/m-p/1596346#M2671</guid>
      <dc:creator>Ben</dc:creator>
      <dc:date>2023-02-09T07:55:27Z</dc:date>
    </item>
    <item>
      <title>Re: 56F837xx ref. design</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/56F837xx-ref-design/m-p/1596450#M2675</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;After you install SDK package, you can load an example as the following procedures:1,2,3,4&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1675934707249.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/210271i6680F67F2BB01E8E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1675934707249.png" alt="xiangjun_rong_0-1675934707249.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Then you can click the Run-&amp;gt;Debug Configuration,then as the following fig&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_1-1675934899328.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/210272iCEA48B040BA304B3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_1-1675934899328.png" alt="xiangjun_rong_1-1675934899328.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;you can download application project to flash.&lt;/P&gt;
&lt;P&gt;If you want to integrate several examples, you can drag the corresponding driver(*.c)&amp;nbsp; and header file(*.h) from SDK package directory to the driver location(location 3 in the first fig) , then you can add the driver code in main().&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Thu, 09 Feb 2023 09:32:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/56F837xx-ref-design/m-p/1596450#M2675</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-02-09T09:32:22Z</dc:date>
    </item>
  </channel>
</rss>