<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal ControllersのトピックRe: 56800EF core</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/56800EF-core/m-p/1583925#M2659</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I see that there is not the reference manual of DSP56800EF core on the website, I will notify the product manager of the fact so that they can post the documentation.&lt;/P&gt;
&lt;P&gt;thank you for pointing out the issue&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Tue, 17 Jan 2023 10:54:40 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2023-01-17T10:54:40Z</dc:date>
    <item>
      <title>56800EF core</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/56800EF-core/m-p/1583868#M2658</link>
      <description>&lt;P&gt;Hello, I've noticed the NXP documentation website lists a new DSC product called &lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/digital-signal-controllers/32-bit-56800ef-dsc-core/dscs-with-integrated-fpu-and-trigonometric-math-engine-with-opamp-and-quadrature-decoder:MC56F80xxx" target="_self"&gt;MC56F80xxx&lt;/A&gt; that uses a new DSC 56800EF core.&lt;BR /&gt;There is no 56800EF documentation but looking in the MC56800xxx generic diagram it seems like it's a 56800EX core with three more units (a single precision FPU, a CORDIC engine and a fast divider) tightly connected to it.&lt;BR /&gt;It's not clear if those units are accessible by way of new instructions or are memory mapped on some peripheral registers.&amp;nbsp;&lt;BR /&gt;Is there more information available or for now it's just a "preview" to reassure MC56F82xxx users that there is a successor for future developments ?&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jan 2023 09:27:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/56800EF-core/m-p/1583868#M2658</guid>
      <dc:creator>Lorenzo_Mch_IT</dc:creator>
      <dc:date>2023-01-17T09:27:20Z</dc:date>
    </item>
    <item>
      <title>Re: 56800EF core</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/56800EF-core/m-p/1583925#M2659</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I see that there is not the reference manual of DSP56800EF core on the website, I will notify the product manager of the fact so that they can post the documentation.&lt;/P&gt;
&lt;P&gt;thank you for pointing out the issue&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jan 2023 10:54:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/56800EF-core/m-p/1583925#M2659</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-01-17T10:54:40Z</dc:date>
    </item>
  </channel>
</rss>