<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: The 56837xx DSP in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/The-56837xx-DSP/m-p/1583842#M2657</link>
    <description>&lt;P&gt;That paragraph generated by chatGPT is factually wrong.&lt;/P&gt;&lt;P&gt;chatGPT is NOT a reliable source, ESPECIALLY when it generates answer to inputs it has no canned correct responses.&lt;/P&gt;&lt;P&gt;Products based on Coldfire architecture use a totally different naming convention and both DSC and DSP devices of the 56-something groups do NOT use Coldfire; for example the 56F8xxxx use Hawk v1,v2,v3 (a.k.a 56800,56800E,56800EX) cores.&lt;/P&gt;</description>
    <pubDate>Tue, 17 Jan 2023 09:02:58 GMT</pubDate>
    <dc:creator>Lorenzo_Mch_IT</dc:creator>
    <dc:date>2023-01-17T09:02:58Z</dc:date>
    <item>
      <title>The 56837xx DSP</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/The-56837xx-DSP/m-p/1583135#M2654</link>
      <description>&lt;P class=""&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;I'm searching for the datasheet of 56837xx core. Can you help me ?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 16 Jan 2023 11:18:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/The-56837xx-DSP/m-p/1583135#M2654</guid>
      <dc:creator>salem1</dc:creator>
      <dc:date>2023-01-16T11:18:58Z</dc:date>
    </item>
    <item>
      <title>Re: The 56837xx DSP</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/The-56837xx-DSP/m-p/1583337#M2655</link>
      <description>&lt;P&gt;Maybe what you are really looking for is &lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/digital-signal-controllers/32-bit-56800ef-dsc-core/performance-level-digital-signal-controllers-usb-fs-otg-can-fd:MC56F83xxx" target="_self"&gt;56&lt;STRONG&gt;F&lt;/STRONG&gt;837xx&lt;/A&gt; ?&amp;nbsp;&lt;BR /&gt;(see the documentation in the link above for datasheets, reference manuals, etc.)&lt;/P&gt;</description>
      <pubDate>Mon, 16 Jan 2023 16:52:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/The-56837xx-DSP/m-p/1583337#M2655</guid>
      <dc:creator>Lorenzo_Mch_IT</dc:creator>
      <dc:date>2023-01-16T16:52:19Z</dc:date>
    </item>
    <item>
      <title>Re: The 56837xx DSP</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/The-56837xx-DSP/m-p/1583388#M2656</link>
      <description>&lt;P&gt;I found this paragraph in chatGPT:&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;&lt;SPAN class=""&gt;The main difference between the MC56F837xx DSP and the 56837xx DSP is their main functionality: the MC56F837xx is a high performance DSP designed for signal processing applications, while the 56837xx is a microcontroller designed for industrial applications, control systems engine, communication systems and on-board systems.

The MC56F837xx uses a 32-bit digital signal processor (DSC) based on the V1 ColdFire+ architecture to deliver high performance in terms of processing speed and power consumption. It is equipped with high-capacity flash memory, advanced communication peripherals, digital I/O, analog-to-digital and digital-to-analog converters, and safety components for industrial, medical, automotive, and automotive applications. communications.

The 56837xx DSP uses the ColdFire V1 architecture, which includes DSP instructions to accelerate common mathematical operations used in signal processing applications, such as filters and Fourier transforms. It is equipped with flash and SRAM memory, communication peripherals, digital inputs/outputs and analog-to-digital converters for conversion&lt;/SPAN&gt;&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 16 Jan 2023 18:05:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/The-56837xx-DSP/m-p/1583388#M2656</guid>
      <dc:creator>salem1</dc:creator>
      <dc:date>2023-01-16T18:05:17Z</dc:date>
    </item>
    <item>
      <title>Re: The 56837xx DSP</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/The-56837xx-DSP/m-p/1583842#M2657</link>
      <description>&lt;P&gt;That paragraph generated by chatGPT is factually wrong.&lt;/P&gt;&lt;P&gt;chatGPT is NOT a reliable source, ESPECIALLY when it generates answer to inputs it has no canned correct responses.&lt;/P&gt;&lt;P&gt;Products based on Coldfire architecture use a totally different naming convention and both DSC and DSP devices of the 56-something groups do NOT use Coldfire; for example the 56F8xxxx use Hawk v1,v2,v3 (a.k.a 56800,56800E,56800EX) cores.&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jan 2023 09:02:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/The-56837xx-DSP/m-p/1583842#M2657</guid>
      <dc:creator>Lorenzo_Mch_IT</dc:creator>
      <dc:date>2023-01-17T09:02:58Z</dc:date>
    </item>
    <item>
      <title>Re: The 56837xx DSP</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/The-56837xx-DSP/m-p/1584560#M2660</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;all the MC56F81xxx, MC56F82xxx, MC56F83xxx, MC56F84xxx use the same core DSP56800EX core. In detail, the MC56F837xx uses the DSP56800EX core.&lt;/P&gt;
&lt;P&gt;Pls download the reference manual of DSP56800EX core from the link:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/digital-signal-controllers/32-bit-56800ef-dsc-core/digital-signal-controllers:MC56F84xxx" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/digital-signal-controllers/32-bit-56800ef-dsc-core/digital-signal-controllers:MC56F84xxx&lt;/A&gt;&lt;/P&gt;
&lt;H3 class="item-title" style="box-sizing: border-box; font-family: 'Nunito Sans', Arial, Helvetica, sans-serif; line-height: 1.1; color: #333f48; margin-top: 0px; margin-bottom: 0px; font-size: 16px; font-weight: bold; position: relative; margin-right: 8px; font-style: normal; font-variant-ligatures: normal; font-variant-caps: normal; letter-spacing: normal; orphans: 2; text-align: left; text-indent: 0px; text-transform: none; white-space: normal; widows: 2; word-spacing: 0px; -webkit-text-stroke-width: 0px; background-color: #ffffff; text-decoration-thickness: initial; text-decoration-style: initial; text-decoration-color: initial;"&gt;&lt;A id="relatedDocsClickPDF_3" class="dtmcustomrulelink" style="box-sizing: border-box; background-color: transparent; color: #215bd6; text-decoration: underline; cursor: pointer; outline: -webkit-focus-ring-color auto 5px; outline-offset: -2px; margin-right: 8px;" href="https://www.nxp.com/webapp/Download?colCode=DSP56800ERM" target="_blank" rel="noopener" data-dtmaction="Documentation Section - Results Link Click" data-dtmsubaction="DSP56800E and DSP56800EX - Reference Manual - NXP - Reference Manual - English"&gt;&lt;SPAN&gt;DSP56800E and DSP56800EX - Reference Manual&lt;/SPAN&gt;&lt;/A&gt;&lt;/H3&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jan 2023 11:11:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/The-56837xx-DSP/m-p/1584560#M2660</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-01-18T11:11:58Z</dc:date>
    </item>
    <item>
      <title>Re: The 56837xx DSP</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/The-56837xx-DSP/m-p/1728685#M2835</link>
      <description>&lt;P&gt;Do you find it useful when using &lt;A href="https://gptdeutsch.de/" target="_blank" rel="noopener"&gt;ChatGPT&lt;/A&gt;? I have used it and it is very useful to me.&lt;/P&gt;</description>
      <pubDate>Mon, 25 Sep 2023 08:04:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/The-56837xx-DSP/m-p/1728685#M2835</guid>
      <dc:creator>fatimahanna</dc:creator>
      <dc:date>2023-09-25T08:04:18Z</dc:date>
    </item>
  </channel>
</rss>