<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal ControllersのトピックSGTL5000: HP_VGND and mic</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/SGTL5000-HP-VGND-and-mic/m-p/1570323#M2640</link>
    <description>&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;I want to use the headset port with HP_VGND. In figure 19("&lt;SPAN class=""&gt;&lt;SPAN&gt;Typical Application Schematic"&lt;/SPAN&gt;&lt;/SPAN&gt;) it is shown that the mic is using GND. My 4 pin headset jack has only one pin for ground so I would get a shortcut of HP_VGND and GND if I would use it in such way. My question is: Is it possible(and reasonable) to use HP_VGND also for the mic?&lt;/P&gt;&lt;P&gt;-Uwe&lt;/P&gt;</description>
    <pubDate>Thu, 15 Dec 2022 09:26:09 GMT</pubDate>
    <dc:creator>UweA</dc:creator>
    <dc:date>2022-12-15T09:26:09Z</dc:date>
    <item>
      <title>SGTL5000: HP_VGND and mic</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/SGTL5000-HP-VGND-and-mic/m-p/1570323#M2640</link>
      <description>&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;I want to use the headset port with HP_VGND. In figure 19("&lt;SPAN class=""&gt;&lt;SPAN&gt;Typical Application Schematic"&lt;/SPAN&gt;&lt;/SPAN&gt;) it is shown that the mic is using GND. My 4 pin headset jack has only one pin for ground so I would get a shortcut of HP_VGND and GND if I would use it in such way. My question is: Is it possible(and reasonable) to use HP_VGND also for the mic?&lt;/P&gt;&lt;P&gt;-Uwe&lt;/P&gt;</description>
      <pubDate>Thu, 15 Dec 2022 09:26:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/SGTL5000-HP-VGND-and-mic/m-p/1570323#M2640</guid>
      <dc:creator>UweA</dc:creator>
      <dc:date>2022-12-15T09:26:09Z</dc:date>
    </item>
    <item>
      <title>Re: SGTL5000: HP_VGND and mic</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/SGTL5000-HP-VGND-and-mic/m-p/1570933#M2641</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I attach the EVK board schematics, pls check the connection.&lt;/P&gt;
&lt;P&gt;I do not think you can connect the HP_VGND to GND directly, pls refer to the Note:&lt;/P&gt;
&lt;P&gt;HP_VGND Note: Do not connect HP_VGND to system ground, even when unused. This is a virtual ground (DC voltage) that should never connect to an actual “0 Volt ground”. Use the widest, shortest trace possible for the HP_VGND.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Fri, 16 Dec 2022 03:32:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/SGTL5000-HP-VGND-and-mic/m-p/1570933#M2641</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-12-16T03:32:25Z</dc:date>
    </item>
    <item>
      <title>Re: SGTL5000: HP_VGND and mic</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/SGTL5000-HP-VGND-and-mic/m-p/1571552#M2643</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26034"&gt;@xiangjun_rong&lt;/a&gt;Thank you for the schematics.&lt;BR /&gt;I know that it is a bad idea to connect HP_VGND to GND. But my question was (and is): Can I use HP_VGND(instead of GND) also for the headset mic?&lt;/P&gt;&lt;P&gt;KR,&lt;BR /&gt;Uwe&lt;/P&gt;</description>
      <pubDate>Sun, 18 Dec 2022 18:11:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/SGTL5000-HP-VGND-and-mic/m-p/1571552#M2643</guid>
      <dc:creator>UweA</dc:creator>
      <dc:date>2022-12-18T18:11:42Z</dc:date>
    </item>
    <item>
      <title>Re: SGTL5000: HP_VGND and mic</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/SGTL5000-HP-VGND-and-mic/m-p/1574551#M2645</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suppose that the HP_VGND is only for the headphone instead of mic.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Dec 2022 09:19:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/SGTL5000-HP-VGND-and-mic/m-p/1574551#M2645</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-12-26T09:19:37Z</dc:date>
    </item>
  </channel>
</rss>