<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC56F8367MPYE, Date code: XAA1315 in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8367MPYE-Date-code-XAA1315/m-p/1546550#M2625</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I have contacted AE team, maybe they know if the batch with date code XAA1315 has issue.&lt;/P&gt;
&lt;P&gt;I will send you a reply after I get feedback.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Tue, 01 Nov 2022 02:20:08 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2022-11-01T02:20:08Z</dc:date>
    <item>
      <title>MC56F8367MPYE, Date code: XAA1315</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8367MPYE-Date-code-XAA1315/m-p/1544315#M2619</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using "MC56F8367MPYE" to control the DC motor and works fine for long time.&lt;/P&gt;&lt;P&gt;Then, we produced the new batch of product and have the following problem:&lt;/P&gt;&lt;P&gt;1) When I power on the chip, it causes MOSFET shortage. I checked the reason and found that some pins of PWMA and PWMB are high after power-on. Based on the datasheet, all PWM channels are disabled after POWER ON or RESET.&lt;/P&gt;&lt;P&gt;2) Date code: XAA1315. Can you tell what it means?&lt;/P&gt;&lt;P&gt;We need to know what the exact problem is and how to fix it?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;</description>
      <pubDate>Wed, 26 Oct 2022 18:46:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8367MPYE-Date-code-XAA1315/m-p/1544315#M2619</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2022-10-26T18:46:59Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F8367MPYE, Date code: XAA1315</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8367MPYE-Date-code-XAA1315/m-p/1544636#M2620</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I think it is common practice to connect 10K ohm pull-down external resistor for each PWM pin, during/after Reset, all the PWM pins are in input mode, the pull-down resistor can pull the pin to LOW, which avoid the damage of the power device because of shortening when you set up the power device in a H bridge.&lt;/P&gt;
&lt;P&gt;BTW, I suppose you know that you have to add dead time for the complementary PWM signals.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Thu, 27 Oct 2022 03:03:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8367MPYE-Date-code-XAA1315/m-p/1544636#M2620</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-10-27T03:03:21Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F8367MPYE, Date code: XAA1315</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8367MPYE-Date-code-XAA1315/m-p/1544637#M2621</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I think it is common practice to connect 10K ohm pull-down external resistor for each PWM pin, during/after Reset, all the PWM pins are in input mode, the pull-down resistor can pull the pin to LOW, which avoid the damage of the power device because of shortening when you set up the power device in a H bridge.&lt;/P&gt;
&lt;P&gt;BTW, I suppose you know that you have to add dead time for the complementary PWM signals.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Thu, 27 Oct 2022 03:03:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8367MPYE-Date-code-XAA1315/m-p/1544637#M2621</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-10-27T03:03:49Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F8367MPYE, Date code: XAA1315</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8367MPYE-Date-code-XAA1315/m-p/1544994#M2622</link>
      <description>&lt;P&gt;Hi XiangJun,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your input. Here are more explanations:&lt;/P&gt;&lt;P&gt;1) It happens on 30% of boards. And these design is used for last several boards and works fine...&lt;/P&gt;&lt;P&gt;2) I have 10K pull-down on all PWM channels.&lt;/P&gt;&lt;P&gt;3) This happens on POWER UP stage, no any software loaded in MCU&lt;/P&gt;&lt;P&gt;4) When I remove MOSFET, no over-current happens.&lt;/P&gt;&lt;P&gt;5) I measured PWM pins, some pins are HIGH. That is the reason causes shortage...&lt;/P&gt;&lt;P&gt;6) I measure the current. When I power ON, it consumes around 130mA, then go up to 160mA, then MOSFET shortage because of HIGH on PWM pins.&lt;/P&gt;&lt;P&gt;I really need your help to see where the problem is and how to fix?&lt;/P&gt;&lt;P&gt;Can I send no function MCU to NXP to confirm?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;</description>
      <pubDate>Thu, 27 Oct 2022 11:39:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8367MPYE-Date-code-XAA1315/m-p/1544994#M2622</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2022-10-27T11:39:45Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F8367MPYE, Date code: XAA1315</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8367MPYE-Date-code-XAA1315/m-p/1545377#M2623</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;does the issue only occur on the branch with data code XAA1315?&lt;/P&gt;
&lt;P&gt;The issue is that the PWM signal are high during the power-up process before any application code is executed, and the external pull-down resistor can not pull the pin to LOW logic, which leads to MOSFET damage during power-up process.&lt;/P&gt;
&lt;P&gt;You can contact local FAE or DFAE, have them to contact failure analysis team.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 28 Oct 2022 02:28:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8367MPYE-Date-code-XAA1315/m-p/1545377#M2623</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-10-28T02:28:22Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F8367MPYE, Date code: XAA1315</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8367MPYE-Date-code-XAA1315/m-p/1545668#M2624</link>
      <description>&lt;P&gt;Hi Xiangjun,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It happens on XAA1315 and XAC1493.&lt;/P&gt;&lt;P&gt;It happens during POWER-UP, no any code is loaded to MCU. The pull-down resistor does not pull down PWM signal.&lt;/P&gt;&lt;P&gt;I am located in Canada, where can I find FAE?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;</description>
      <pubDate>Fri, 28 Oct 2022 11:50:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8367MPYE-Date-code-XAA1315/m-p/1545668#M2624</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2022-10-28T11:50:19Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F8367MPYE, Date code: XAA1315</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8367MPYE-Date-code-XAA1315/m-p/1546550#M2625</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I have contacted AE team, maybe they know if the batch with date code XAA1315 has issue.&lt;/P&gt;
&lt;P&gt;I will send you a reply after I get feedback.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Tue, 01 Nov 2022 02:20:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8367MPYE-Date-code-XAA1315/m-p/1546550#M2625</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-11-01T02:20:08Z</dc:date>
    </item>
  </channel>
</rss>