<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal Controllers中的主题 Re: MC56F83783 support</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F83783-support/m-p/1530830#M2610</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Regarding the pin configuration, I suggest you write the peripheral register directly.&lt;/P&gt;
&lt;P&gt;This is an example to configure the pin as PWM function.&lt;/P&gt;
&lt;P&gt;Secondly, you can call the SDK api function for example:&lt;/P&gt;
&lt;P&gt;void BOARD_InitPins(void)&lt;BR /&gt;{&lt;BR /&gt;/* GPIOC IPBus Clock Enable: The peripheral is clocked. */&lt;BR /&gt;CLOCK_EnableClock(kCLOCK_GPIOC);&lt;BR /&gt;/* GPIOD IPBus Clock Enable: The peripheral is clocked. */&lt;BR /&gt;CLOCK_EnableClock(kCLOCK_GPIOD);&lt;BR /&gt;/* Enable peripheral functionality on pin GPIOC0 (pin 3) */&lt;BR /&gt;GPIO_PinSetPeripheralMode(BOARD_EXTAL_GPIO, BOARD_EXTAL_PIN_MASK, kGPIO_ModePeripheral);&lt;BR /&gt;/* Peripheral functionality on pin GPIOC0 (pin 3) */&lt;BR /&gt;GPIO_PinSetPeripheralMux(kGPIO_Peri_C0_EXTAL);&lt;BR /&gt;/* Enable peripheral functionality on pin GPIOC1 (pin 4) */&lt;BR /&gt;GPIO_PinSetPeripheralMode(BOARD_XTAL_GPIO, BOARD_XTAL_PIN_MASK, kGPIO_ModePeripheral);&lt;BR /&gt;/* Enable peripheral functionality on pin GPIOD5 (pin 10) */&lt;BR /&gt;GPIO_PinSetPeripheralMode(BOARD_RXD_BDM_GPIO, BOARD_RXD_BDM_PIN_MASK, kGPIO_ModePeripheral);&lt;BR /&gt;/* Peripheral functionality on pin GPIOD5 (pin 10) */&lt;BR /&gt;GPIO_PinSetPeripheralMux(kGPIO_Peri_D5_RXD2);&lt;BR /&gt;/* Enable peripheral functionality on pin GPIOD6 (pin 9) */&lt;BR /&gt;GPIO_PinSetPeripheralMode(BOARD_TXD_BDM_GPIO, BOARD_TXD_BDM_PIN_MASK, kGPIO_ModePeripheral);&lt;BR /&gt;/* Peripheral functionality on pin GPIOD6 (pin 9) */&lt;BR /&gt;GPIO_PinSetPeripheralMux(kGPIO_Peri_D6_TXD2);&lt;BR /&gt;}&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;void PWMPinAssignment(void)&lt;BR /&gt;{&lt;BR /&gt;//enable gated clock for GPIOE and GPIUOG port&lt;BR /&gt;SIM-&amp;gt;PCE0|=1&amp;lt;&amp;lt;2|1&amp;lt;&amp;lt;0;&lt;BR /&gt;GPIOE-&amp;gt;PER|=0x3F;&lt;BR /&gt;GPIOG-&amp;gt;PER|=1&amp;lt;&amp;lt;5;&lt;BR /&gt;//clear E0/E1/E2/E3/E4/E5 bits&lt;BR /&gt;SIM-&amp;gt;GPSEL&amp;amp;=~(0xFFF);&lt;BR /&gt;//set up the G5 as 2b'01&lt;BR /&gt;SIM-&amp;gt;GPSGL&amp;amp;=~(0xC00);&lt;BR /&gt;SIM-&amp;gt;GPSGL|=1&amp;lt;&amp;lt;10;&lt;BR /&gt;&lt;BR /&gt;}&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;//use GPIOG6 as GPIO output signal, which can be a PWM fault signal&lt;BR /&gt;//GPIOG6 pin pin11 of J4&lt;BR /&gt;void GpioG6_GPIOOUTPUT_Init(void)&lt;BR /&gt;{&lt;BR /&gt;//enable GPIOG port clock&lt;BR /&gt;SIM-&amp;gt;PCE0|=1&amp;lt;&amp;lt;0;&lt;BR /&gt;//clear the GPIOG6 bit in PER reg&lt;BR /&gt;GPIOG-&amp;gt;PER&amp;amp;=~(0x40);&lt;BR /&gt;GPIOG-&amp;gt;DDR|=1&amp;lt;&amp;lt;6;&lt;BR /&gt;GPIOG-&amp;gt;DR=GPIOG-&amp;gt;DR^0x40;&lt;BR /&gt;__asm(nop);&lt;BR /&gt;GPIOG-&amp;gt;DR=GPIOG-&amp;gt;DR^0x40;&lt;/P&gt;
&lt;P&gt;}&lt;/P&gt;
&lt;P&gt;//the PIT0 cycle time is 0.5s&lt;BR /&gt;void PIT0_Init(void)&lt;BR /&gt;{&lt;BR /&gt;//enable PIT0 gated clock&lt;BR /&gt;SIM-&amp;gt;PCE2|=1&amp;lt;&amp;lt;3;&lt;BR /&gt;//PIT0 prescaler is 32768, the PIT0 cycl;e time is (100 000 000/32768)=3051&lt;BR /&gt;PIT0-&amp;gt;CTRL=0x0F&amp;lt;&amp;lt;3;&lt;BR /&gt;PIT0-&amp;gt;MOD=1525;&lt;BR /&gt;PIT0-&amp;gt;CTRL|=0x03;&lt;BR /&gt;INTC-&amp;gt;IPR10|=3&amp;lt;&amp;lt;12;&lt;BR /&gt;}&lt;BR /&gt;#pragma interrupt on&lt;BR /&gt;void PIT0_ISR(void)&lt;BR /&gt;{&lt;BR /&gt;//clear the flag of PIT0&lt;BR /&gt;&lt;BR /&gt;PIT0-&amp;gt;CTRL&amp;amp;=~(0x01&amp;lt;&amp;lt;2);&lt;BR /&gt;//toggle led0&lt;BR /&gt;__asm(nop);&lt;BR /&gt;GPIOG-&amp;gt;DR=GPIOG-&amp;gt;DR^0x40;&lt;BR /&gt;}&lt;BR /&gt;#pragma interrupt off&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Fri, 30 Sep 2022 03:21:51 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2022-09-30T03:21:51Z</dc:date>
    <item>
      <title>MC56F83783 support</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F83783-support/m-p/1527009#M2599</link>
      <description>&lt;P&gt;How can I add MC56F83783 to CW for MCU v11.1? (+PE support)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 22 Sep 2022 23:29:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F83783-support/m-p/1527009#M2599</guid>
      <dc:creator>Ben</dc:creator>
      <dc:date>2022-09-22T23:29:38Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F83783 support</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F83783-support/m-p/1527035#M2600</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Pls download CodeWarrior for MCU ver10.x from the link and install it on your PC.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-legacy/codewarrior-for-mcus-eclipse-ide-coldfire-56800-e-dsc-qorivva-56xx-rs08-s08-s12z-11-1:CW-MCU10" target="_blank"&gt;https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-legacy/codewarrior-for-mcus-eclipse-ide-coldfire-56800-e-dsc-qorivva-56xx-rs08-s08-s12z-11-1:CW-MCU10&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For the patch installation, I attach a doc, but I suppose the doc is very old.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 23 Sep 2022 01:22:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F83783-support/m-p/1527035#M2600</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-09-23T01:22:43Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F83783 support</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F83783-support/m-p/1527195#M2601</link>
      <description>&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Do you mean that ver. 10 support this chip and ver 11 doesnt?&lt;/P&gt;&lt;P&gt;I think that ver. 10 is older than this chip&lt;/P&gt;&lt;P&gt;please explain&lt;/P&gt;</description>
      <pubDate>Fri, 23 Sep 2022 07:45:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F83783-support/m-p/1527195#M2601</guid>
      <dc:creator>Ben</dc:creator>
      <dc:date>2022-09-23T07:45:57Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F83783 support</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F83783-support/m-p/1527257#M2602</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I am sorry, it was my mistake, I suggest you download latest version of CodeWarrior for MCU ver11.1 instead of version 10.x.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-legacy/codewarrior-for-mcus-eclipse-ide-coldfire-56800-e-dsc-qorivva-56xx-rs08-s08-s12z-11-1:CW-MCU10?_gl=1*u32s4y*_ga*NTYzNzEwODc1LjE2NjM4OTU2NzY.*_ga_WM5LE0KMSH*MTY2MzkxNzY5NC40LjEuMTY2MzkyMjg4OS4wLjAuMA." target="_blank"&gt;https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-legacy/codewarrior-for-mcus-eclipse-ide-coldfire-56800-e-dsc-qorivva-56xx-rs08-s08-s12z-11-1:CW-MCU10?_gl=1*u32s4y*_ga*NTYzNzEwODc1LjE2NjM4OTU2NzY.*_ga_WM5LE0KMSH*MTY2MzkxNzY5NC40LjEuMTY2MzkyMjg4OS4wLjAuMA.&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;I suppose that&amp;nbsp; maybe version 11.1 supports MC56F83xxx, you do not need install patch.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Fri, 23 Sep 2022 08:54:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F83783-support/m-p/1527257#M2602</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-09-23T08:54:36Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F83783 support</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F83783-support/m-p/1527675#M2603</link>
      <description>&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;I am using ver 11.1, so I installed the last updates 3 and 4 and now I can open new project with this chip. BUT: there is no internal PE support for the chip, and I can not see it in the processors library list.&lt;/P&gt;&lt;P&gt;Is there any add-on I should install to get full support for this chip (MC56F83783)?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 25 Sep 2022 14:48:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F83783-support/m-p/1527675#M2603</guid>
      <dc:creator>Ben</dc:creator>
      <dc:date>2022-09-25T14:48:24Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F83783 support</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F83783-support/m-p/1527742#M2604</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Unfortunately, the MC56F83xxx no longer supports PE, now all MCU uses SDK package to develop code.&lt;/P&gt;
&lt;P&gt;Pls download SDK package from the link based on MC56F83xxx.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-software-development-kit-sdk:MCUXpresso-SDK" target="_blank"&gt;https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-software-development-kit-sdk:MCUXpresso-SDK&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Sep 2022 02:02:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F83783-support/m-p/1527742#M2604</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-09-26T02:02:51Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F83783 support</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F83783-support/m-p/1529498#M2605</link>
      <description>&lt;P&gt;Thanks Rong,&lt;/P&gt;&lt;P&gt;I tried to work with the xpresso before. I dont like the config activity: I had to enter the online tool, define the I/O and modules, then pack it to installation file and install it on my computer.&lt;/P&gt;&lt;P&gt;This works good, but what happens if I want to change the I/O? do I have to enter the config tool again and install a new project on my computer? what about all the code I already wrote?&lt;/P&gt;&lt;P&gt;Please guide me if there is another way to make changes.&lt;/P&gt;</description>
      <pubDate>Wed, 28 Sep 2022 11:03:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F83783-support/m-p/1529498#M2605</guid>
      <dc:creator>Ben</dc:creator>
      <dc:date>2022-09-28T11:03:24Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F83783 support</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F83783-support/m-p/1530830#M2610</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Regarding the pin configuration, I suggest you write the peripheral register directly.&lt;/P&gt;
&lt;P&gt;This is an example to configure the pin as PWM function.&lt;/P&gt;
&lt;P&gt;Secondly, you can call the SDK api function for example:&lt;/P&gt;
&lt;P&gt;void BOARD_InitPins(void)&lt;BR /&gt;{&lt;BR /&gt;/* GPIOC IPBus Clock Enable: The peripheral is clocked. */&lt;BR /&gt;CLOCK_EnableClock(kCLOCK_GPIOC);&lt;BR /&gt;/* GPIOD IPBus Clock Enable: The peripheral is clocked. */&lt;BR /&gt;CLOCK_EnableClock(kCLOCK_GPIOD);&lt;BR /&gt;/* Enable peripheral functionality on pin GPIOC0 (pin 3) */&lt;BR /&gt;GPIO_PinSetPeripheralMode(BOARD_EXTAL_GPIO, BOARD_EXTAL_PIN_MASK, kGPIO_ModePeripheral);&lt;BR /&gt;/* Peripheral functionality on pin GPIOC0 (pin 3) */&lt;BR /&gt;GPIO_PinSetPeripheralMux(kGPIO_Peri_C0_EXTAL);&lt;BR /&gt;/* Enable peripheral functionality on pin GPIOC1 (pin 4) */&lt;BR /&gt;GPIO_PinSetPeripheralMode(BOARD_XTAL_GPIO, BOARD_XTAL_PIN_MASK, kGPIO_ModePeripheral);&lt;BR /&gt;/* Enable peripheral functionality on pin GPIOD5 (pin 10) */&lt;BR /&gt;GPIO_PinSetPeripheralMode(BOARD_RXD_BDM_GPIO, BOARD_RXD_BDM_PIN_MASK, kGPIO_ModePeripheral);&lt;BR /&gt;/* Peripheral functionality on pin GPIOD5 (pin 10) */&lt;BR /&gt;GPIO_PinSetPeripheralMux(kGPIO_Peri_D5_RXD2);&lt;BR /&gt;/* Enable peripheral functionality on pin GPIOD6 (pin 9) */&lt;BR /&gt;GPIO_PinSetPeripheralMode(BOARD_TXD_BDM_GPIO, BOARD_TXD_BDM_PIN_MASK, kGPIO_ModePeripheral);&lt;BR /&gt;/* Peripheral functionality on pin GPIOD6 (pin 9) */&lt;BR /&gt;GPIO_PinSetPeripheralMux(kGPIO_Peri_D6_TXD2);&lt;BR /&gt;}&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;void PWMPinAssignment(void)&lt;BR /&gt;{&lt;BR /&gt;//enable gated clock for GPIOE and GPIUOG port&lt;BR /&gt;SIM-&amp;gt;PCE0|=1&amp;lt;&amp;lt;2|1&amp;lt;&amp;lt;0;&lt;BR /&gt;GPIOE-&amp;gt;PER|=0x3F;&lt;BR /&gt;GPIOG-&amp;gt;PER|=1&amp;lt;&amp;lt;5;&lt;BR /&gt;//clear E0/E1/E2/E3/E4/E5 bits&lt;BR /&gt;SIM-&amp;gt;GPSEL&amp;amp;=~(0xFFF);&lt;BR /&gt;//set up the G5 as 2b'01&lt;BR /&gt;SIM-&amp;gt;GPSGL&amp;amp;=~(0xC00);&lt;BR /&gt;SIM-&amp;gt;GPSGL|=1&amp;lt;&amp;lt;10;&lt;BR /&gt;&lt;BR /&gt;}&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;//use GPIOG6 as GPIO output signal, which can be a PWM fault signal&lt;BR /&gt;//GPIOG6 pin pin11 of J4&lt;BR /&gt;void GpioG6_GPIOOUTPUT_Init(void)&lt;BR /&gt;{&lt;BR /&gt;//enable GPIOG port clock&lt;BR /&gt;SIM-&amp;gt;PCE0|=1&amp;lt;&amp;lt;0;&lt;BR /&gt;//clear the GPIOG6 bit in PER reg&lt;BR /&gt;GPIOG-&amp;gt;PER&amp;amp;=~(0x40);&lt;BR /&gt;GPIOG-&amp;gt;DDR|=1&amp;lt;&amp;lt;6;&lt;BR /&gt;GPIOG-&amp;gt;DR=GPIOG-&amp;gt;DR^0x40;&lt;BR /&gt;__asm(nop);&lt;BR /&gt;GPIOG-&amp;gt;DR=GPIOG-&amp;gt;DR^0x40;&lt;/P&gt;
&lt;P&gt;}&lt;/P&gt;
&lt;P&gt;//the PIT0 cycle time is 0.5s&lt;BR /&gt;void PIT0_Init(void)&lt;BR /&gt;{&lt;BR /&gt;//enable PIT0 gated clock&lt;BR /&gt;SIM-&amp;gt;PCE2|=1&amp;lt;&amp;lt;3;&lt;BR /&gt;//PIT0 prescaler is 32768, the PIT0 cycl;e time is (100 000 000/32768)=3051&lt;BR /&gt;PIT0-&amp;gt;CTRL=0x0F&amp;lt;&amp;lt;3;&lt;BR /&gt;PIT0-&amp;gt;MOD=1525;&lt;BR /&gt;PIT0-&amp;gt;CTRL|=0x03;&lt;BR /&gt;INTC-&amp;gt;IPR10|=3&amp;lt;&amp;lt;12;&lt;BR /&gt;}&lt;BR /&gt;#pragma interrupt on&lt;BR /&gt;void PIT0_ISR(void)&lt;BR /&gt;{&lt;BR /&gt;//clear the flag of PIT0&lt;BR /&gt;&lt;BR /&gt;PIT0-&amp;gt;CTRL&amp;amp;=~(0x01&amp;lt;&amp;lt;2);&lt;BR /&gt;//toggle led0&lt;BR /&gt;__asm(nop);&lt;BR /&gt;GPIOG-&amp;gt;DR=GPIOG-&amp;gt;DR^0x40;&lt;BR /&gt;}&lt;BR /&gt;#pragma interrupt off&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Fri, 30 Sep 2022 03:21:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F83783-support/m-p/1530830#M2610</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-09-30T03:21:51Z</dc:date>
    </item>
  </channel>
</rss>