<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PCA9615DXP communication failure in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9615DXP-communication-failure/m-p/1509890#M2576</link>
    <description>&lt;P&gt;1: No more issue for your schematic,but VDD pin need decouple capacitor such as 22uF+100nF.&lt;/P&gt;&lt;P&gt;2: suggest you test the function and performance on PCB no the breadboard.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 23 Aug 2022 05:19:06 GMT</pubDate>
    <dc:creator>guoweisun</dc:creator>
    <dc:date>2022-08-23T05:19:06Z</dc:date>
    <item>
      <title>PCA9615DXP communication failure</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9615DXP-communication-failure/m-p/1507463#M2568</link>
      <description>&lt;P&gt;Dear forum,&lt;/P&gt;&lt;P&gt;I am struggling with 2x PCA9615 to communicate. My test setup consists out of 2x arduino and 2x PCA9615. The master arduino has been given address 11 and the slave has been given 12.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Di2c bus is connected using jumper wires on a breadboard, same goes for the i2c bus. Between the DxxxP/DxxxM busses is a 120ohm resistor, with 680ohm resistors pulling the DxxxP side to Vdd and DxxxM to Vss (like in the documentation). I also put an extra 10kOhm resistor on the enable pin to Vdd, but this should not be necessary as the chip has it's own pullup resistor.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Putting the i2c bus directly from the master to the slave functions as intended, data can be interchanged.&lt;/P&gt;&lt;P&gt;Thank you very much in advance.&lt;/P&gt;</description>
      <pubDate>Wed, 17 Aug 2022 11:07:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9615DXP-communication-failure/m-p/1507463#M2568</guid>
      <dc:creator>kvuurens</dc:creator>
      <dc:date>2022-08-17T11:07:05Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9615DXP communication failure</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9615DXP-communication-failure/m-p/1507550#M2569</link>
      <description>&lt;P&gt;I debugged some more and after hooking the oscilloscope up to the output of the differential chip I do not see any activity on the line. Looks like the chip is not enabled?&lt;BR /&gt;&lt;BR /&gt;I've tried 4 different chips to exclude the risk that I've burned the chips while soldering. Chips also are from a reputable reseller (mouser electronics).&lt;/P&gt;</description>
      <pubDate>Wed, 17 Aug 2022 14:13:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9615DXP-communication-failure/m-p/1507550#M2569</guid>
      <dc:creator>kvuurens</dc:creator>
      <dc:date>2022-08-17T14:13:07Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9615DXP communication failure</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9615DXP-communication-failure/m-p/1508422#M2570</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kvuurens_0-1660853676036.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/190652i7B970FEA2BFA65F0/image-size/large?v=v2&amp;amp;px=999" role="button" title="kvuurens_0-1660853676036.png" alt="kvuurens_0-1660853676036.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;After using the logic analyser I see that the DSDA works, but the DSCL does not. DSCLM is low as you can see in the screenshot and DSCLP is high, as per the documentation.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;The "slave" in the screenshot is actually functioning as a master using I2C terms, which is tring to get data from 0x0C (address 12). Any idea why the DSCL pair is not doing anything? I checked loose wiring etc, but could not find anything..&lt;BR /&gt;&lt;BR /&gt;Also; the actual data part is empty as seen below on the screenshot:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kvuurens_1-1660854197179.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/190653iD3607BDD9753DE24/image-size/large?v=v2&amp;amp;px=999" role="button" title="kvuurens_1-1660854197179.png" alt="kvuurens_1-1660854197179.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;To add; other chips have the same behaviour. Swapping SDA and SCL on the I2C side does result in the switching of the signal of the differential side (I2C SDA on SCL input, giving DSCL on the line).&lt;/P&gt;</description>
      <pubDate>Thu, 18 Aug 2022 20:46:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9615DXP-communication-failure/m-p/1508422#M2570</guid>
      <dc:creator>kvuurens</dc:creator>
      <dc:date>2022-08-18T20:46:45Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9615DXP communication failure</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9615DXP-communication-failure/m-p/1509194#M2572</link>
      <description>&lt;P&gt;Please give your schematic here!&lt;/P&gt;</description>
      <pubDate>Mon, 22 Aug 2022 05:50:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9615DXP-communication-failure/m-p/1509194#M2572</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2022-08-22T05:50:05Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9615DXP communication failure</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9615DXP-communication-failure/m-p/1509727#M2575</link>
      <description>&lt;P&gt;Dear Guoweisun,&lt;BR /&gt;&lt;BR /&gt;see below. I've only added one termination resistor set, as it's on the same breadboard, max 20cm apart from eachother. Currently not using twisted pair, but will be used in the final solution. All +5V and GND is on the same rail.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="kvuurens_0-1661205005471.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/190917i6D01A78947C781A9/image-size/large?v=v2&amp;amp;px=999" role="button" title="kvuurens_0-1661205005471.png" alt="kvuurens_0-1661205005471.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Aug 2022 21:54:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9615DXP-communication-failure/m-p/1509727#M2575</guid>
      <dc:creator>kvuurens</dc:creator>
      <dc:date>2022-08-22T21:54:16Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9615DXP communication failure</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9615DXP-communication-failure/m-p/1509890#M2576</link>
      <description>&lt;P&gt;1: No more issue for your schematic,but VDD pin need decouple capacitor such as 22uF+100nF.&lt;/P&gt;&lt;P&gt;2: suggest you test the function and performance on PCB no the breadboard.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Aug 2022 05:19:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9615DXP-communication-failure/m-p/1509890#M2576</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2022-08-23T05:19:06Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9615DXP communication failure</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9615DXP-communication-failure/m-p/1510401#M2578</link>
      <description>&lt;P&gt;Hi Guo,&lt;BR /&gt;&lt;BR /&gt;the decouple capacitor did the trick. Data is flowing. Got one question; I do not see the "differential" part of the dI2C like it is in the documentation, both for SDA and SCL:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kvuurens_0-1661285709412.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/191040i9C0CAB3FD8EE65A9/image-size/large?v=v2&amp;amp;px=999" role="button" title="kvuurens_0-1661285709412.png" alt="kvuurens_0-1661285709412.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;When I remove the 100Ohm resistor (seen on the screenshot marked by the red stripe), I do see the differential part, but the data (obviously) stops flowing:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kvuurens_1-1661285870396.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/191041i884763368D44A6DA/image-size/large?v=v2&amp;amp;px=999" role="button" title="kvuurens_1-1661285870396.png" alt="kvuurens_1-1661285870396.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Aug 2022 20:18:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9615DXP-communication-failure/m-p/1510401#M2578</guid>
      <dc:creator>kvuurens</dc:creator>
      <dc:date>2022-08-23T20:18:40Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9615DXP communication failure</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9615DXP-communication-failure/m-p/1513273#M2579</link>
      <description>&lt;P&gt;So this issue that is shown above really is blocking me, when I use twisted pair instead of jumper wires it stops communicating.&lt;/P&gt;</description>
      <pubDate>Mon, 29 Aug 2022 15:01:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9615DXP-communication-failure/m-p/1513273#M2579</guid>
      <dc:creator>kvuurens</dc:creator>
      <dc:date>2022-08-29T15:01:17Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9615DXP communication failure</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9615DXP-communication-failure/m-p/1517536#M2580</link>
      <description>&lt;P&gt;Anybody got an idea about this?&lt;/P&gt;</description>
      <pubDate>Tue, 06 Sep 2022 08:35:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9615DXP-communication-failure/m-p/1517536#M2580</guid>
      <dc:creator>kvuurens</dc:creator>
      <dc:date>2022-09-06T08:35:26Z</dc:date>
    </item>
  </channel>
</rss>