<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic BLDC demo code for DSC 56F81XXX or 82XXX in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/BLDC-demo-code-for-DSC-56F81XXX-or-82XXX/m-p/1508940#M2571</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp; We need to upgrade our BLDC speed controller with 16bit MC56F8135 to 32bits DSC like 81XXX or 82XXX. I have the EVK boards such as MC56F81000-EVK and TWR-56F8200 with FRDM-MC-LVBLDC and APMOTOR56F8000e. Any demo code for my upgrade project with my kits&lt;/P&gt;&lt;P&gt;I also saw a good demo as below&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxpic.org.cn/module/forum/thread-621561-1-1.html" target="_blank"&gt;https://www.nxpic.org.cn/module/forum/thread-621561-1-1.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Any demo code for it?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Fred&lt;/P&gt;</description>
    <pubDate>Fri, 19 Aug 2022 17:30:24 GMT</pubDate>
    <dc:creator>Fred_Liu</dc:creator>
    <dc:date>2022-08-19T17:30:24Z</dc:date>
    <item>
      <title>BLDC demo code for DSC 56F81XXX or 82XXX</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/BLDC-demo-code-for-DSC-56F81XXX-or-82XXX/m-p/1508940#M2571</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp; We need to upgrade our BLDC speed controller with 16bit MC56F8135 to 32bits DSC like 81XXX or 82XXX. I have the EVK boards such as MC56F81000-EVK and TWR-56F8200 with FRDM-MC-LVBLDC and APMOTOR56F8000e. Any demo code for my upgrade project with my kits&lt;/P&gt;&lt;P&gt;I also saw a good demo as below&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxpic.org.cn/module/forum/thread-621561-1-1.html" target="_blank"&gt;https://www.nxpic.org.cn/module/forum/thread-621561-1-1.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Any demo code for it?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Fred&lt;/P&gt;</description>
      <pubDate>Fri, 19 Aug 2022 17:30:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/BLDC-demo-code-for-DSC-56F81XXX-or-82XXX/m-p/1508940#M2571</guid>
      <dc:creator>Fred_Liu</dc:creator>
      <dc:date>2022-08-19T17:30:24Z</dc:date>
    </item>
    <item>
      <title>Re: BLDC demo code for DSC 56F81XXX or 82XXX</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/BLDC-demo-code-for-DSC-56F81XXX-or-82XXX/m-p/1509223#M2573</link>
      <description>&lt;P&gt;Hi, Fred,&lt;/P&gt;
&lt;P&gt;As you know that there are two on-chip OPAMPs for MC56F81xxx family, if you use the MC56F81000-EVK plus FRDM-MC-LVBLDC , the on-chip two OPAMPs are not used, we have not the example code to control BLDC with the two OPAMPs involved.&lt;/P&gt;
&lt;P&gt;If you are interested in the OPAMP utilization, we have the example code in SDK package:&lt;/P&gt;
&lt;P&gt;...........\SDK_2_10_0_MC56F81000-EVK\boards\mc56f81000evk\driver_examples\opamp&lt;/P&gt;
&lt;P&gt;You can download the SDK package for MC56F81xxx from the link:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://mcuxpresso.nxp.com/en/welcome" target="_blank"&gt;https://mcuxpresso.nxp.com/en/welcome&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BTW, there are two dedicated OPAMP on the FRDM-MC-LVBLDC, I suppose that you can use the on-chip OPAMP to replace them.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Aug 2022 06:19:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/BLDC-demo-code-for-DSC-56F81XXX-or-82XXX/m-p/1509223#M2573</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-08-22T06:19:39Z</dc:date>
    </item>
  </channel>
</rss>