<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal ControllersのトピックRe: PTN36043, Can I cross SS1, SS2?</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PTN36043-Can-I-cross-SS1-SS2/m-p/1498391#M2561</link>
    <description>&lt;P&gt;Could you please give the connection diagram?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 31 Jul 2022 23:37:48 GMT</pubDate>
    <dc:creator>guoweisun</dc:creator>
    <dc:date>2022-07-31T23:37:48Z</dc:date>
    <item>
      <title>PTN36043, Can I cross SS1, SS2?</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PTN36043-Can-I-cross-SS1-SS2/m-p/1495859#M2556</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I plan to connect all USB SS lines using two PTN36043.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to use TX1 and RT2/TX2 and RX1 as a pair because the artwork design is distorted. Is there a problem with the operation when it is connected like this?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;TX1 RX2 - PTN36043 #1 -&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;TX2 RX1 - PTN36043 #2 -&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jul 2022 00:06:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/PTN36043-Can-I-cross-SS1-SS2/m-p/1495859#M2556</guid>
      <dc:creator>Jeong</dc:creator>
      <dc:date>2022-07-27T00:06:49Z</dc:date>
    </item>
    <item>
      <title>Re: PTN36043, Can I cross SS1, SS2?</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PTN36043-Can-I-cross-SS1-SS2/m-p/1498391#M2561</link>
      <description>&lt;P&gt;Could you please give the connection diagram?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 31 Jul 2022 23:37:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/PTN36043-Can-I-cross-SS1-SS2/m-p/1498391#M2561</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2022-07-31T23:37:48Z</dc:date>
    </item>
  </channel>
</rss>