<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I need Static bootloader source code for MC56F8037 in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/I-need-Static-bootloader-source-code-for-MC56F8037/m-p/1495468#M2554</link>
    <description>&lt;P&gt;Thanks for the detailed and kind explanation.&lt;/P&gt;</description>
    <pubDate>Tue, 26 Jul 2022 09:03:34 GMT</pubDate>
    <dc:creator>laonnuri</dc:creator>
    <dc:date>2022-07-26T09:03:34Z</dc:date>
    <item>
      <title>I need Static bootloader source code for MC56F8037</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/I-need-Static-bootloader-source-code-for-MC56F8037/m-p/1493740#M2546</link>
      <description>&lt;P&gt;anyone please help&lt;/P&gt;&lt;P&gt;I can't find the static_bootloader source code for the MC56F8037.&lt;BR /&gt;Can you tell me where I can get the download or provide the static_bootloader source code?&lt;/P&gt;</description>
      <pubDate>Fri, 22 Jul 2022 04:14:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/I-need-Static-bootloader-source-code-for-MC56F8037/m-p/1493740#M2546</guid>
      <dc:creator>laonnuri</dc:creator>
      <dc:date>2022-07-22T04:14:00Z</dc:date>
    </item>
    <item>
      <title>Re: I need Static bootloader source code for MC56F8037</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/I-need-Static-bootloader-source-code-for-MC56F8037/m-p/1495196#M2549</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As you know that the MC56F803x is a bit old(released in 2009 year), the bootloader can be generated with the CodeWarrior for DSP56800E ver8.3 as the following screenshot, after you click File-&amp;gt;New-&amp;gt;Processor Expert Examples Stationery&lt;/P&gt;
&lt;P&gt;Then select the bootloader, the tools will generate the bootloader code based on the selected DSC derivatives.&lt;/P&gt;
&lt;P&gt;But the CodeWarrior for DSP56800E ver8.3&amp;nbsp; has issue if you run it on Win 10 OS, because the tools has not updated for a long time. Pls get a PC with Win XP OS and install the CodeWarrior for DSP56800E ver8.3 tools.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1658806136310.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/187785iE4FD82972537A48E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1658806136310.png" alt="xiangjun_rong_0-1658806136310.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jul 2022 03:35:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/I-need-Static-bootloader-source-code-for-MC56F8037/m-p/1495196#M2549</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-07-26T03:35:59Z</dc:date>
    </item>
    <item>
      <title>Re: I need Static bootloader source code for MC56F8037</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/I-need-Static-bootloader-source-code-for-MC56F8037/m-p/1495228#M2550</link>
      <description>&lt;P&gt;Thanks for your kind reply.&lt;/P&gt;&lt;P&gt;However, the serial_bootloader generated via "Processor Expert Examples Stationery" is known as a dynamic_booltloader that runs after the code has been moved from FLASH to RAM.&lt;/P&gt;&lt;P&gt;I'd appreciate it if you could confirm that the method you described is how to create a static serial bootloader that can be run continuously in FLASH.&lt;/P&gt;&lt;P&gt;And I know that you provided static_serial_bootloader source code as "~.zip" in the past.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jul 2022 04:57:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/I-need-Static-bootloader-source-code-for-MC56F8037/m-p/1495228#M2550</guid>
      <dc:creator>laonnuri</dc:creator>
      <dc:date>2022-07-26T04:57:37Z</dc:date>
    </item>
    <item>
      <title>Re: I need Static bootloader source code for MC56F8037</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/I-need-Static-bootloader-source-code-for-MC56F8037/m-p/1495323#M2551</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;pls refer to the AN4275.pdf for the static/dynamic bootloader for MC56F82xx.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jul 2022 07:03:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/I-need-Static-bootloader-source-code-for-MC56F8037/m-p/1495323#M2551</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-07-26T07:03:09Z</dc:date>
    </item>
    <item>
      <title>Re: I need Static bootloader source code for MC56F8037</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/I-need-Static-bootloader-source-code-for-MC56F8037/m-p/1495371#M2552</link>
      <description>&lt;P&gt;Thanks for your kind reply.&lt;/P&gt;&lt;P&gt;If so, can you tell me what part I need to modify to omit "copy RAM code and data from flash to RAM" in the "flowchart" below and make "RAM code" run in flash?&lt;BR /&gt;(source code? or make_file? or start_code?)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="flow.jpg" style="width: 724px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/187828i7EB7964A431C4DA0/image-size/large?v=v2&amp;amp;px=999" role="button" title="flow.jpg" alt="flow.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jul 2022 07:47:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/I-need-Static-bootloader-source-code-for-MC56F8037/m-p/1495371#M2552</guid>
      <dc:creator>laonnuri</dc:creator>
      <dc:date>2022-07-26T07:47:29Z</dc:date>
    </item>
    <item>
      <title>Re: I need Static bootloader source code for MC56F8037</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/I-need-Static-bootloader-source-code-for-MC56F8037/m-p/1495409#M2553</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The MC56F803x has just 32KW(64K bytes) flash, all the flash is located in the one block, if you want to operate the flash(erasing/programming), the code to erase flash/program flash in bootloader must be located in program RAM and run from program RAM to operate flash so that the application binary can be programmed in flash by bootloader.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jul 2022 08:28:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/I-need-Static-bootloader-source-code-for-MC56F8037/m-p/1495409#M2553</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-07-26T08:28:08Z</dc:date>
    </item>
    <item>
      <title>Re: I need Static bootloader source code for MC56F8037</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/I-need-Static-bootloader-source-code-for-MC56F8037/m-p/1495468#M2554</link>
      <description>&lt;P&gt;Thanks for the detailed and kind explanation.&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jul 2022 09:03:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/I-need-Static-bootloader-source-code-for-MC56F8037/m-p/1495468#M2554</guid>
      <dc:creator>laonnuri</dc:creator>
      <dc:date>2022-07-26T09:03:34Z</dc:date>
    </item>
  </channel>
</rss>