<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal Controllers中的主题 Re: Clock generation in CAN bus devices</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Clock-generation-in-CAN-bus-devices/m-p/1490246#M2543</link>
    <description>&lt;P&gt;The data sheet says "microcontroller&amp;#2;independent clock source" is present on the chip, but where can further details be taken from?&lt;/P&gt;</description>
    <pubDate>Fri, 15 Jul 2022 10:07:13 GMT</pubDate>
    <dc:creator>rknispel</dc:creator>
    <dc:date>2022-07-15T10:07:13Z</dc:date>
    <item>
      <title>Clock generation in CAN bus devices</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Clock-generation-in-CAN-bus-devices/m-p/1489527#M2536</link>
      <description>&lt;P&gt;I am looking for details of the clock generation in UJA1169ATK/F:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;clock source&lt;/LI&gt;&lt;LI&gt;PLL&lt;/LI&gt;&lt;LI&gt;Jitter in 13 bit interval of CAN communications&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Is there a technology papaer where it can be derived from?&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jul 2022 13:45:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Clock-generation-in-CAN-bus-devices/m-p/1489527#M2536</guid>
      <dc:creator>rknispel</dc:creator>
      <dc:date>2022-07-14T13:45:10Z</dc:date>
    </item>
    <item>
      <title>Re: Clock generation in CAN bus devices</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Clock-generation-in-CAN-bus-devices/m-p/1490246#M2543</link>
      <description>&lt;P&gt;The data sheet says "microcontroller&amp;#2;independent clock source" is present on the chip, but where can further details be taken from?&lt;/P&gt;</description>
      <pubDate>Fri, 15 Jul 2022 10:07:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Clock-generation-in-CAN-bus-devices/m-p/1490246#M2543</guid>
      <dc:creator>rknispel</dc:creator>
      <dc:date>2022-07-15T10:07:13Z</dc:date>
    </item>
    <item>
      <title>Re: Clock generation in CAN bus devices</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Clock-generation-in-CAN-bus-devices/m-p/1490625#M2544</link>
      <description>&lt;P&gt;What kinds of clock detail information do you need?&lt;/P&gt;</description>
      <pubDate>Mon, 18 Jul 2022 00:10:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Clock-generation-in-CAN-bus-devices/m-p/1490625#M2544</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2022-07-18T00:10:40Z</dc:date>
    </item>
    <item>
      <title>Re: Clock generation in CAN bus devices</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Clock-generation-in-CAN-bus-devices/m-p/1490998#M2545</link>
      <description>&lt;P&gt;My questionnaire is about details of the Automotive qualification of the CAN communications of UJA1169ATK/F:&lt;/P&gt;&lt;P&gt;CAN network clock source&lt;BR /&gt;PLL frequency [MHz]&lt;BR /&gt;max. PLL jitter in 13 bit interval&lt;BR /&gt;oscillator manufacturer&lt;BR /&gt;oscillator part name&lt;BR /&gt;oscillator frequency [MHz]&lt;BR /&gt;oscillator tolerance [%]&lt;/P&gt;&lt;P&gt;Possible answers include clock recovery from CANH/CANL lines, and the oscillator would be MCU oscillator.&lt;/P&gt;</description>
      <pubDate>Mon, 18 Jul 2022 10:32:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Clock-generation-in-CAN-bus-devices/m-p/1490998#M2545</guid>
      <dc:creator>rknispel</dc:creator>
      <dc:date>2022-07-18T10:32:55Z</dc:date>
    </item>
    <item>
      <title>Re: Clock generation in CAN bus devices</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Clock-generation-in-CAN-bus-devices/m-p/1493818#M2547</link>
      <description>&lt;P&gt;These parameters should be checked or setting in CAN controller side,right?UJA1169 is CAN&amp;nbsp;transceiver.&lt;/P&gt;</description>
      <pubDate>Fri, 22 Jul 2022 06:55:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Clock-generation-in-CAN-bus-devices/m-p/1493818#M2547</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2022-07-22T06:55:07Z</dc:date>
    </item>
    <item>
      <title>Re: Clock generation in CAN bus devices</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Clock-generation-in-CAN-bus-devices/m-p/1493967#M2548</link>
      <description>&lt;P&gt;The parameters are relevant for reliabilty of CAN communications in on-board network as Automotive application. UJA1169 is considered for SBC of such a component.&lt;/P&gt;&lt;P&gt;Typically the internal clock is generated from TXD by clock recovery. I am looking for more details on this process!&lt;/P&gt;&lt;P&gt;Help is very much appreciated and thanks for any hints in advance!&lt;/P&gt;</description>
      <pubDate>Fri, 22 Jul 2022 09:49:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Clock-generation-in-CAN-bus-devices/m-p/1493967#M2548</guid>
      <dc:creator>rknispel</dc:creator>
      <dc:date>2022-07-22T09:49:48Z</dc:date>
    </item>
    <item>
      <title>Re: Clock generation in CAN bus devices</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Clock-generation-in-CAN-bus-devices/m-p/1495481#M2555</link>
      <description>&lt;P&gt;The question was transferred into a service case and resolved there.&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jul 2022 09:25:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Clock-generation-in-CAN-bus-devices/m-p/1495481#M2555</guid>
      <dc:creator>rknispel</dc:creator>
      <dc:date>2022-07-26T09:25:45Z</dc:date>
    </item>
  </channel>
</rss>