<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Solenoid Controller in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Solenoid-Controller/m-p/1469789#M2516</link>
    <description>&lt;P&gt;I new to KIT33816board and I am using it to do the injection. Now, I want to control the behavior of injection and pumping control valve in LABView since some feedback signals which are used to do a closed loop control come into the LABView. But here is problem, how can I run different single command or batch command automatically after I change the parameters in the configuration registers?&lt;/P&gt;</description>
    <pubDate>Tue, 07 Jun 2022 07:23:59 GMT</pubDate>
    <dc:creator>whalex</dc:creator>
    <dc:date>2022-06-07T07:23:59Z</dc:date>
    <item>
      <title>Solenoid Controller</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Solenoid-Controller/m-p/1469789#M2516</link>
      <description>&lt;P&gt;I new to KIT33816board and I am using it to do the injection. Now, I want to control the behavior of injection and pumping control valve in LABView since some feedback signals which are used to do a closed loop control come into the LABView. But here is problem, how can I run different single command or batch command automatically after I change the parameters in the configuration registers?&lt;/P&gt;</description>
      <pubDate>Tue, 07 Jun 2022 07:23:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Solenoid-Controller/m-p/1469789#M2516</guid>
      <dc:creator>whalex</dc:creator>
      <dc:date>2022-06-07T07:23:59Z</dc:date>
    </item>
    <item>
      <title>Re: Solenoid Controller</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Solenoid-Controller/m-p/1470338#M2519</link>
      <description>&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/user-guide/MC33816DSWUG.pdf" target="_blank"&gt;MC33816DSWUG, MC33816 Developer Studio User’s Guide - User’s Guide (nxp.com.cn)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Above is the&amp;nbsp;MC33816 Developer Studio,hope this could help you!&lt;/P&gt;</description>
      <pubDate>Wed, 08 Jun 2022 04:04:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Solenoid-Controller/m-p/1470338#M2519</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2022-06-08T04:04:27Z</dc:date>
    </item>
  </channel>
</rss>