<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal Controllers中的主题 Is Freemaster supported on the 56F8037?</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Is-Freemaster-supported-on-the-56F8037/m-p/350321#M248</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Customer is having issues getting Freemaster to work with a 56F8037. Is a serial or CAN connection recommended?&lt;/P&gt;&lt;P&gt;What versions of CodeWarrior&amp;nbsp; are compatible with both? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Sep 2014 13:45:27 GMT</pubDate>
    <dc:creator>Larry5335</dc:creator>
    <dc:date>2014-09-09T13:45:27Z</dc:date>
    <item>
      <title>Is Freemaster supported on the 56F8037?</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Is-Freemaster-supported-on-the-56F8037/m-p/350321#M248</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Customer is having issues getting Freemaster to work with a 56F8037. Is a serial or CAN connection recommended?&lt;/P&gt;&lt;P&gt;What versions of CodeWarrior&amp;nbsp; are compatible with both? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Sep 2014 13:45:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Is-Freemaster-supported-on-the-56F8037/m-p/350321#M248</guid>
      <dc:creator>Larry5335</dc:creator>
      <dc:date>2014-09-09T13:45:27Z</dc:date>
    </item>
    <item>
      <title>Re: Is Freemaster supported on the 56F8037?</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Is-Freemaster-supported-on-the-56F8037/m-p/350322#M249</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Freemaster supports&amp;nbsp; the connection with 56F8037 through JTAG or SCI interface. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;User can use either Classic CodeWarrior v8.3 or Eclipse&amp;nbsp; CodeWarrior v10.6&amp;nbsp; to develop the application which supports Freemaster connection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Processor Expert contains two beans for FreeMaster communication, one is PC_Master, the other is FreeMaster. For SCI connection, you can choose either of them. For JTAG connection (using parallel or USBTAP), you can only choose FreeMaster. &lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Fiona&lt;/P&gt;&lt;P&gt;Technical Information &amp;amp; Commercial Support&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Sep 2014 03:15:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Is-Freemaster-supported-on-the-56F8037/m-p/350322#M249</guid>
      <dc:creator>TICS_Fiona</dc:creator>
      <dc:date>2014-09-10T03:15:44Z</dc:date>
    </item>
  </channel>
</rss>