<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC56F8006: How to generate two phase shift PWM signals? in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8006-How-to-generate-two-phase-shift-PWM-signals/m-p/349477#M247</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;At first really thank you for share your knowledge about this topic and was really useful. Now i'm trying to make this situation but applied to a 3 phase shift PWM signals, and this case of course for get 120 degrees of shifting. Can i use the same logic? But using the 3 complementary pair of PWM?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the same logic, i used a valur of PWM_CMOD = 22400 , so i split that value in 6 fractions. &lt;/P&gt;&lt;P&gt;PWM_VAL0 = 0;&lt;/P&gt;&lt;P&gt;PWM_VAL1 = 22400 * (1/5);&lt;/P&gt;&lt;P&gt;PWM_VAL1 = 22400 * (2/5);&lt;/P&gt;&lt;P&gt;.....&lt;/P&gt;&lt;P&gt;PWM_VAL5 = 22400 * (5/5);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Should i use at same edge-align-complementary? Why instead of center-align ??&lt;/P&gt;&lt;P&gt;Is it correct?? It´s a really important academical project, and i need be sure in relation of this.&lt;/P&gt;&lt;P&gt;Thank you in advance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Jun 2015 17:53:38 GMT</pubDate>
    <dc:creator>ruimausinho</dc:creator>
    <dc:date>2015-06-17T17:53:38Z</dc:date>
    <item>
      <title>MC56F8006: How to generate two phase shift PWM signals?</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8006-How-to-generate-two-phase-shift-PWM-signals/m-p/349475#M245</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dears,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to generate two PWM signals to control an inverter. They must be equals (same duty cycle) with a phase shift of 180°. Can anyone give an idea on how to solve this issue?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 14 Dec 2014 14:44:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8006-How-to-generate-two-phase-shift-PWM-signals/m-p/349475#M245</guid>
      <dc:creator>CarlosCba</dc:creator>
      <dc:date>2014-12-14T14:44:05Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F8006: How to generate two phase shift PWM signals?</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8006-How-to-generate-two-phase-shift-PWM-signals/m-p/349476#M246</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Carlos dL,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Regarding your question that you want to use PWM of MC56F8006 to control a an inverter with push-pull layout, I think it is okay, you can connect PWM0 to one MOSFET, connect PWM2 to another MOSFET, PWM1 and PWM3 are not used.&lt;/P&gt;&lt;P&gt; You can set up the PWM0/PWM1 pair in complenmentary mode, PWM2/PWM3 pair in complementary mode, I suggest you use edge-alignment mode, while you set the PCE0 and PCE1 bits in PWM_ICCTRL register. If the PCE0 and PCE1 bits are set, you can use VAL0 and VAL1 to control the rising/falling edge of PWM0 and use VAL2 and VAL3 to control rising and falling edge of PWM2 signals, PWM1 and PWM3 are not used in application.&lt;/P&gt;&lt;P&gt; for example, if the PWM_CMOD=1000, you can set PWM_VAL0=0, PWM_VAL1=250, set PWM_VAL2=500,PWM_VAL3=750, in the above setting, both PWM0/PWM2 will have 25% duty cycle and phase shift 180.&lt;/P&gt;&lt;P&gt; Pls refer to an3844.pdf which can be downloaded from the website:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://tinyurl.com/kcdrkll"&gt;http://tinyurl.com/kcdrkll&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Best Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Xiangjun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Dec 2014 08:52:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8006-How-to-generate-two-phase-shift-PWM-signals/m-p/349476#M246</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2014-12-18T08:52:12Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F8006: How to generate two phase shift PWM signals?</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8006-How-to-generate-two-phase-shift-PWM-signals/m-p/349477#M247</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;At first really thank you for share your knowledge about this topic and was really useful. Now i'm trying to make this situation but applied to a 3 phase shift PWM signals, and this case of course for get 120 degrees of shifting. Can i use the same logic? But using the 3 complementary pair of PWM?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the same logic, i used a valur of PWM_CMOD = 22400 , so i split that value in 6 fractions. &lt;/P&gt;&lt;P&gt;PWM_VAL0 = 0;&lt;/P&gt;&lt;P&gt;PWM_VAL1 = 22400 * (1/5);&lt;/P&gt;&lt;P&gt;PWM_VAL1 = 22400 * (2/5);&lt;/P&gt;&lt;P&gt;.....&lt;/P&gt;&lt;P&gt;PWM_VAL5 = 22400 * (5/5);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Should i use at same edge-align-complementary? Why instead of center-align ??&lt;/P&gt;&lt;P&gt;Is it correct?? It´s a really important academical project, and i need be sure in relation of this.&lt;/P&gt;&lt;P&gt;Thank you in advance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jun 2015 17:53:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8006-How-to-generate-two-phase-shift-PWM-signals/m-p/349477#M247</guid>
      <dc:creator>ruimausinho</dc:creator>
      <dc:date>2015-06-17T17:53:38Z</dc:date>
    </item>
  </channel>
</rss>