<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Splitter IC in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Splitter-IC/m-p/1425664#M2456</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Please double check whether CBTL06DP213 multiplexing meet your requirement or not.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 10 Mar 2022 00:18:40 GMT</pubDate>
    <dc:creator>guoweisun</dc:creator>
    <dc:date>2022-03-10T00:18:40Z</dc:date>
    <item>
      <title>Splitter IC</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Splitter-IC/m-p/1424710#M2454</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Do you have an IC that can output 1 HDMI input as 2 HDMI outputs (min 4K with HDCP support) at the same time (both outputs active at the same time)? The output should be able to run two different brands and models of monitors at the same time.&lt;/P&gt;&lt;P&gt;Which of your products can we use?&lt;/P&gt;&lt;P&gt;Best Regards;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Mar 2022 16:39:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Splitter-IC/m-p/1424710#M2454</guid>
      <dc:creator>Pınar</dc:creator>
      <dc:date>2022-03-08T16:39:52Z</dc:date>
    </item>
    <item>
      <title>Re: Splitter IC</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Splitter-IC/m-p/1425664#M2456</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Please double check whether CBTL06DP213 multiplexing meet your requirement or not.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Mar 2022 00:18:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Splitter-IC/m-p/1425664#M2456</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2022-03-10T00:18:40Z</dc:date>
    </item>
    <item>
      <title>Re: Splitter IC</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Splitter-IC/m-p/1425815#M2457</link>
      <description>&lt;P&gt;Hi there;&lt;/P&gt;&lt;P&gt;If I'm not misinterpreting the datasheet; It is emphasized that only one channel can be selected. We need two active outputs that can output simultaneously.&lt;/P&gt;&lt;P&gt;For example, the circuit whose picture I have attached/shared below provides output to both a 4K HDMI 2.0 (with HDCP) monitor and a VGA monitor at the same time.&lt;/P&gt;&lt;P&gt;We are designing a similar device. Both monitors must be turned on.&lt;/P&gt;&lt;P&gt;We are looking for an IC that can send images to both devices.&lt;/P&gt;</description>
      <pubDate>Thu, 10 Mar 2022 05:00:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Splitter-IC/m-p/1425815#M2457</guid>
      <dc:creator>Pınar</dc:creator>
      <dc:date>2022-03-10T05:00:40Z</dc:date>
    </item>
    <item>
      <title>Re: Splitter IC</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Splitter-IC/m-p/1426438#M2459</link>
      <description>&lt;P&gt;Seems no suitable part!&lt;/P&gt;</description>
      <pubDate>Fri, 11 Mar 2022 01:03:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Splitter-IC/m-p/1426438#M2459</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2022-03-11T01:03:48Z</dc:date>
    </item>
  </channel>
</rss>