<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal Controllers中的主题 82748 program on specific address in internal flash</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/82748-program-on-specific-address-in-internal-flash/m-p/1416495#M2432</link>
    <description>&lt;P&gt;Dear NXP expert,&lt;/P&gt;&lt;P&gt;How can i program on&amp;nbsp; specific address in internal flash? 0x7c00~0x7fff is the calibration data, I shouldn't&amp;nbsp; erase the sector when I update the program. Now when I program the chip, it will always erase the whole flash.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 21 Feb 2022 06:23:12 GMT</pubDate>
    <dc:creator>terrybogard</dc:creator>
    <dc:date>2022-02-21T06:23:12Z</dc:date>
    <item>
      <title>82748 program on specific address in internal flash</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/82748-program-on-specific-address-in-internal-flash/m-p/1416495#M2432</link>
      <description>&lt;P&gt;Dear NXP expert,&lt;/P&gt;&lt;P&gt;How can i program on&amp;nbsp; specific address in internal flash? 0x7c00~0x7fff is the calibration data, I shouldn't&amp;nbsp; erase the sector when I update the program. Now when I program the chip, it will always erase the whole flash.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Feb 2022 06:23:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/82748-program-on-specific-address-in-internal-flash/m-p/1416495#M2432</guid>
      <dc:creator>terrybogard</dc:creator>
      <dc:date>2022-02-21T06:23:12Z</dc:date>
    </item>
    <item>
      <title>Re: 82748 program on specific address in internal flash</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/82748-program-on-specific-address-in-internal-flash/m-p/1416653#M2433</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suppose that the ADC calibration data is from application code, I think this is workaround.&lt;/P&gt;
&lt;P&gt;You can do calibration and after the calibration, you can save the calibration data to a SRAM in debug mode or whatever, then record or copy the calibration data. You can create a new project, declare the&amp;nbsp; a constant array which is initialized with the calibration ADC data, in the new project, you can read the constant data and write them to ADC register.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Feb 2022 09:30:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/82748-program-on-specific-address-in-internal-flash/m-p/1416653#M2433</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-02-21T09:30:57Z</dc:date>
    </item>
  </channel>
</rss>