<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal Controllers中的主题 Re: Can only Transmit over the Serial Communication Interface, when connected to Debugger.</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Can-only-Transmit-over-the-Serial-Communication-Interface-when/m-p/1400205#M2384</link>
    <description>&lt;P&gt;Great. That was the issue. Writting twice to the MODRR0 rgister&lt;/P&gt;</description>
    <pubDate>Mon, 17 Jan 2022 09:50:29 GMT</pubDate>
    <dc:creator>malikos</dc:creator>
    <dc:date>2022-01-17T09:50:29Z</dc:date>
    <item>
      <title>Can only Transmit over the Serial Communication Interface, when connected to Debugger.</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Can-only-Transmit-over-the-Serial-Communication-Interface-when/m-p/1397417#M2374</link>
      <description>&lt;P&gt;I am currently using a MC9S12ZVM Family. I am trying to transmit some data over the serial communication interface (via Lin). However I can only successfully transmit the data when I am connected to Code Warrior and when the debugging session is active. I do not want to use the debugger when transmitting the data (would do it via Canoe). Is there a way of configuring the SCI so that you do not need to use the debugger to send the information over the SCI.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I attach my configuration&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jan 2022 13:25:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Can-only-Transmit-over-the-Serial-Communication-Interface-when/m-p/1397417#M2374</guid>
      <dc:creator>malikos</dc:creator>
      <dc:date>2022-01-11T13:25:13Z</dc:date>
    </item>
    <item>
      <title>Re: Can only Transmit over the Serial Communication Interface, when connected to Debugger.</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Can-only-Transmit-over-the-Serial-Communication-Interface-when/m-p/1398714#M2377</link>
      <description>&lt;P&gt;Any ideas? The serial communication interface is&amp;nbsp;Serial Communication Interface (S12SCIV6)&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jan 2022 08:00:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Can-only-Transmit-over-the-Serial-Communication-Interface-when/m-p/1398714#M2377</guid>
      <dc:creator>malikos</dc:creator>
      <dc:date>2022-01-13T08:00:40Z</dc:date>
    </item>
    <item>
      <title>Re: Can only Transmit over the Serial Communication Interface, when connected to Debugger.</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Can-only-Transmit-over-the-Serial-Communication-Interface-when/m-p/1400020#M2383</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;it smells like there is something initialized twice and is allowed to be only once.&lt;/P&gt;
&lt;P&gt;You use Processor Expert setup and believe you made some adjustment.&lt;/P&gt;
&lt;P&gt;Some registers are write once only. For example MODRR, CPMUCOP register which routes peripherals to pins. When you use normal mode (no BDM) the if it is set for the first time then it is not re-writable.&lt;/P&gt;
&lt;P&gt;Moreover, you only describe it does not communicate. Have you tested the MCU is working and not still in the reset phase or in loop start-reset caused by COP setup...write once only?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Mon, 17 Jan 2022 07:18:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Can-only-Transmit-over-the-Serial-Communication-Interface-when/m-p/1400020#M2383</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2022-01-17T07:18:45Z</dc:date>
    </item>
    <item>
      <title>Re: Can only Transmit over the Serial Communication Interface, when connected to Debugger.</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Can-only-Transmit-over-the-Serial-Communication-Interface-when/m-p/1400205#M2384</link>
      <description>&lt;P&gt;Great. That was the issue. Writting twice to the MODRR0 rgister&lt;/P&gt;</description>
      <pubDate>Mon, 17 Jan 2022 09:50:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Can-only-Transmit-over-the-Serial-Communication-Interface-when/m-p/1400205#M2384</guid>
      <dc:creator>malikos</dc:creator>
      <dc:date>2022-01-17T09:50:29Z</dc:date>
    </item>
  </channel>
</rss>