<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NVT2002 application issue in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/NVT2002-application-issue/m-p/1332745#M2236</link>
    <description>&lt;P&gt;Hello NXP team:&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Recently, I used NVT2002DP to change the I2C signal level from 5V to 3.3V, details are that I2C master(NXP MCU 5V) on VerB, I2C device(3V3) on VerA according to reference design, but I have one issue, which is as below: when I2C master send the message to the device, I found that the&amp;nbsp;VerB side waveform is normal, but on VerA side, the waveform is distorted , and the high level(3V3) cannot be down to low level(0V) normally(you can check the waveform), could you please help me resolve the issue? Thanks a lot!&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 01 Sep 2021 00:32:16 GMT</pubDate>
    <dc:creator>PhenixYu</dc:creator>
    <dc:date>2021-09-01T00:32:16Z</dc:date>
    <item>
      <title>NVT2002 application issue</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/NVT2002-application-issue/m-p/1332745#M2236</link>
      <description>&lt;P&gt;Hello NXP team:&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Recently, I used NVT2002DP to change the I2C signal level from 5V to 3.3V, details are that I2C master(NXP MCU 5V) on VerB, I2C device(3V3) on VerA according to reference design, but I have one issue, which is as below: when I2C master send the message to the device, I found that the&amp;nbsp;VerB side waveform is normal, but on VerA side, the waveform is distorted , and the high level(3V3) cannot be down to low level(0V) normally(you can check the waveform), could you please help me resolve the issue? Thanks a lot!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 01 Sep 2021 00:32:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/NVT2002-application-issue/m-p/1332745#M2236</guid>
      <dc:creator>PhenixYu</dc:creator>
      <dc:date>2021-09-01T00:32:16Z</dc:date>
    </item>
    <item>
      <title>Re: NVT2002 application issue</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/NVT2002-application-issue/m-p/1332868#M2238</link>
      <description>&lt;P&gt;Please use 1.74K resistors on B side for pull up to 5V.&lt;/P&gt;</description>
      <pubDate>Wed, 01 Sep 2021 04:57:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/NVT2002-application-issue/m-p/1332868#M2238</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2021-09-01T04:57:02Z</dc:date>
    </item>
  </channel>
</rss>