<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Quadrature Output Pulse Generation using Timers with 56F82748 in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Quadrature-Output-Pulse-Generation-using-Timers-with-56F82748/m-p/1313146#M2219</link>
    <description>&lt;P&gt;How to generate Quadrature output pulse using eflex pwm with DSC MC56F8247 controller using CodeWarrior v10.6.&lt;/P&gt;</description>
    <pubDate>Mon, 26 Jul 2021 09:29:45 GMT</pubDate>
    <dc:creator>manikandanb</dc:creator>
    <dc:date>2021-07-26T09:29:45Z</dc:date>
    <item>
      <title>Quadrature Output Pulse Generation using Timers with 56F82748</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Quadrature-Output-Pulse-Generation-using-Timers-with-56F82748/m-p/798318#M1314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How Can i generate Stream of Pulses(based on the speed at which my motor is spinning) which are to be quadrature in nature with Timers (Say Timer 0 &amp;amp; 1) with DSC 56F82748VLL. Also, Change the direction of Pulses based on the Direction of rotation. (This function is same as emulated encoder pulses. But to be generated from MCU) .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jul 2018 11:11:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Quadrature-Output-Pulse-Generation-using-Timers-with-56F82748/m-p/798318#M1314</guid>
      <dc:creator>sandeepn</dc:creator>
      <dc:date>2018-07-30T11:11:26Z</dc:date>
    </item>
    <item>
      <title>Re: Quadrature Output Pulse Generation using Timers with 56F82748</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Quadrature-Output-Pulse-Generation-using-Timers-with-56F82748/m-p/798319#M1315</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Sandeep,&lt;/P&gt;&lt;P&gt;I think you can use eFlexPWM module to generate the two signal with 90 degree shift, as the eFlexPWM has the function to generate the Phase Shifted PWMs.&lt;/P&gt;&lt;P&gt;I think you can use quadtimer to generate the two signal with 90 degree shift, when one timer is master, the other is slave. But it is easier to use eFlexPWM module.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;B R&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Jul 2018 05:32:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Quadrature-Output-Pulse-Generation-using-Timers-with-56F82748/m-p/798319#M1315</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2018-07-31T05:32:24Z</dc:date>
    </item>
    <item>
      <title>Re: Quadrature Output Pulse Generation using Timers with 56F82748</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Quadrature-Output-Pulse-Generation-using-Timers-with-56F82748/m-p/1313146#M2219</link>
      <description>&lt;P&gt;How to generate Quadrature output pulse using eflex pwm with DSC MC56F8247 controller using CodeWarrior v10.6.&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jul 2021 09:29:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Quadrature-Output-Pulse-Generation-using-Timers-with-56F82748/m-p/1313146#M2219</guid>
      <dc:creator>manikandanb</dc:creator>
      <dc:date>2021-07-26T09:29:45Z</dc:date>
    </item>
  </channel>
</rss>