<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal ControllersのトピックNeed information regarding cell controller BMS</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Need-information-regarding-cell-controller-BMS/m-p/1291661#M2188</link>
    <description>&lt;P&gt;Dear Team,&lt;/P&gt;&lt;P&gt;As per the Application note for&amp;nbsp;MC33772B Passive cell balancing also included inside the Evaluation board. please replay the below query.&lt;/P&gt;&lt;P&gt;1. Is it possible to get only the sensing module without the passive balancing?&lt;/P&gt;&lt;P&gt;2. Even if passive balancing included with the controller ..is it possible to bypass the passive balancing section?&lt;/P&gt;&lt;P&gt;3. is there any NXP board available for Active cell balancing?&lt;/P&gt;&lt;P&gt;4. Is there any module for lithium-ion battery voltage, current, and temperature sensing?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Pratyay&lt;/P&gt;</description>
    <pubDate>Sun, 13 Jun 2021 09:50:43 GMT</pubDate>
    <dc:creator>pratayay123</dc:creator>
    <dc:date>2021-06-13T09:50:43Z</dc:date>
    <item>
      <title>Need information regarding cell controller BMS</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Need-information-regarding-cell-controller-BMS/m-p/1291661#M2188</link>
      <description>&lt;P&gt;Dear Team,&lt;/P&gt;&lt;P&gt;As per the Application note for&amp;nbsp;MC33772B Passive cell balancing also included inside the Evaluation board. please replay the below query.&lt;/P&gt;&lt;P&gt;1. Is it possible to get only the sensing module without the passive balancing?&lt;/P&gt;&lt;P&gt;2. Even if passive balancing included with the controller ..is it possible to bypass the passive balancing section?&lt;/P&gt;&lt;P&gt;3. is there any NXP board available for Active cell balancing?&lt;/P&gt;&lt;P&gt;4. Is there any module for lithium-ion battery voltage, current, and temperature sensing?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Pratyay&lt;/P&gt;</description>
      <pubDate>Sun, 13 Jun 2021 09:50:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Need-information-regarding-cell-controller-BMS/m-p/1291661#M2188</guid>
      <dc:creator>pratayay123</dc:creator>
      <dc:date>2021-06-13T09:50:43Z</dc:date>
    </item>
    <item>
      <title>Re: Need information regarding cell controller BMS</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Need-information-regarding-cell-controller-BMS/m-p/1295200#M2194</link>
      <description>&lt;P&gt;For your questions the answer are NO.&lt;/P&gt;</description>
      <pubDate>Mon, 21 Jun 2021 06:42:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Need-information-regarding-cell-controller-BMS/m-p/1295200#M2194</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2021-06-21T06:42:19Z</dc:date>
    </item>
  </channel>
</rss>