<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal ControllersのトピックRe: MC56F8355 start-up</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8355-start-up/m-p/1262406#M2113</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Generally, you can use digital 3.3V(connected to VDDIO) to generate analog 3.3V(connected to VDDA) via a ferrite bead, while, you can connect a ferrite bead between VSS and VSSA.&lt;/P&gt;
&lt;P&gt;I have checked the data sheet of MC56F8355, I have not seen the power-up sequence requirement for VDDIO and VDDA.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Xiangjun Rong&lt;/P&gt;</description>
    <pubDate>Thu, 15 Apr 2021 02:21:30 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2021-04-15T02:21:30Z</dc:date>
    <item>
      <title>MC56F8355 start-up</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8355-start-up/m-p/1248866#M2075</link>
      <description>Hello, I have an issue about MC56F8355 start-up: - the internal voltage is equal to 2,5V and stable - the external Reset rises up after 173ms - the external clock is a cristal at 8Mhz and the amplitude signal is about 2V - the RSTO output rises up 20µs after Reset The DSC can start-up a few times but not at each time When the DSC doesn't start-up, the CLKO output is low Could you help me ? Thank you in advanced Regards Christophe</description>
      <pubDate>Fri, 19 Mar 2021 10:51:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8355-start-up/m-p/1248866#M2075</guid>
      <dc:creator>christophe_c</dc:creator>
      <dc:date>2021-03-19T10:51:27Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F8355 start-up</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8355-start-up/m-p/1249223#M2079</link>
      <description>&lt;P&gt;Hi, Christophe,&lt;/P&gt;
&lt;P&gt;It appears that the crystal works unreliably, pls refer to the configuration I copied from Data sheet:&lt;/P&gt;
&lt;P&gt;From software, you have to set the OCCS_OSCTL[COHL]=1.&lt;/P&gt;
&lt;P&gt;Pls add two caps on the EXTAL/XTAL pins and have a try. If you still have question, pls change another 8MHz crystal from different manufacturer.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1616376034008.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/140225iA3BE0CFCCC8A1AF2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1616376034008.png" alt="xiangjun_rong_0-1616376034008.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Mar 2021 01:30:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8355-start-up/m-p/1249223#M2079</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-03-22T01:30:00Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F8355 start-up</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8355-start-up/m-p/1262025#M2112</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I tried different crystal manufacturers, I tried a ceramic resonator and I applyed an external clock but the result is the same&lt;/P&gt;&lt;P&gt;I found a new information :&lt;/P&gt;&lt;P&gt;If I put a delay of 100ms between VddIO and Vdda_ADC, the DSC starts-up.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The VddIO has to apply after Vdda_ADC of the DSC.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have you an explanation about that ?&lt;/P&gt;</description>
      <pubDate>Wed, 14 Apr 2021 12:54:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8355-start-up/m-p/1262025#M2112</guid>
      <dc:creator>christophe_c</dc:creator>
      <dc:date>2021-04-14T12:54:10Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F8355 start-up</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8355-start-up/m-p/1262406#M2113</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Generally, you can use digital 3.3V(connected to VDDIO) to generate analog 3.3V(connected to VDDA) via a ferrite bead, while, you can connect a ferrite bead between VSS and VSSA.&lt;/P&gt;
&lt;P&gt;I have checked the data sheet of MC56F8355, I have not seen the power-up sequence requirement for VDDIO and VDDA.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Xiangjun Rong&lt;/P&gt;</description>
      <pubDate>Thu, 15 Apr 2021 02:21:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8355-start-up/m-p/1262406#M2113</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-04-15T02:21:30Z</dc:date>
    </item>
  </channel>
</rss>