<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal ControllersのトピックRe: PCA9517 5V Voltage Tolerant</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9517-5V-Voltage-Tolerant/m-p/1246796#M2065</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;EN is pull up to VCCB internal of IC,you can feed VCCB/EN as 3.3V SDAB/SCLB pull up to VCCB,and SDAA/SCLA pull up to VCCA 5V.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 17 Mar 2021 03:03:29 GMT</pubDate>
    <dc:creator>guoweisun</dc:creator>
    <dc:date>2021-03-17T03:03:29Z</dc:date>
    <item>
      <title>PCA9517 5V Voltage Tolerant</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9517-5V-Voltage-Tolerant/m-p/1246283#M2061</link>
      <description>&lt;P&gt;I checked the datasheet for the PCA9517. It stated that the PCA9517 is 5V tolerant.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The PCA9517 is 5 V tolerant, so it does not require any additional circuitry to translate&lt;BR /&gt;between 0.9 V to 5.5 V bus voltages and 2.7 V to 5.5 V bus voltages.&lt;/P&gt;&lt;P&gt;If I want to translate 3.3V to 5V I2C. Can I feed 5V to EN, VCCA and VCCB? instead of having two-level of voltages feed into VCCA and VCCB?&lt;/P&gt;&lt;P&gt;diagram attached for illustration.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;</description>
      <pubDate>Tue, 16 Mar 2021 08:58:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9517-5V-Voltage-Tolerant/m-p/1246283#M2061</guid>
      <dc:creator>zulkifliaziz</dc:creator>
      <dc:date>2021-03-16T08:58:04Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9517 5V Voltage Tolerant</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9517-5V-Voltage-Tolerant/m-p/1246796#M2065</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;EN is pull up to VCCB internal of IC,you can feed VCCB/EN as 3.3V SDAB/SCLB pull up to VCCB,and SDAA/SCLA pull up to VCCA 5V.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Mar 2021 03:03:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/PCA9517-5V-Voltage-Tolerant/m-p/1246796#M2065</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2021-03-17T03:03:29Z</dc:date>
    </item>
  </channel>
</rss>